How to build Native ARM compiler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to build Native ARM compiler

1,469件の閲覧回数
Raana
Contributor III

Dear All,

Currently, I'm working with i.Mx6 SODIMM custom board. (OS: Linux - Yocto)

There, I want to build the Native ARM compiler to compile my application on my target board itself.

Is it possible?

If it so, can any one share the procedure to build that.

Thanks in Advance.

Best Regards,

J.P.Raja

ラベル(3)
0 件の賞賛
返信
1 返信

1,323件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Raana,

First add the following packet in your <build_dir>/conf/local.conf file

IMAGE_INSTALL_append += "\

packagegroup-sdk-target \

"

The build (bitbake) your image.

Finally, when your image is up and running in your custom board you can use the command below to build.

arm-poky-linux-gnueabi-g++ fileName -o outputFileName


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信