I would like to amend the dhcp, how to do it?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I would like to amend the dhcp, how to do it?

1,155件の閲覧回数
qiubin2012
Contributor I

CPU:IMX6S   Kernel:Linux3.0.35  

The board is powered on and configured with static IP. I would like to amend the dhcp, how to do it?

タグ(3)
0 件の賞賛
返信
1 返信

913件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello彬 丘,

You may edit the IP configuration on the kernel boot arguments.

You can see the options available on Table 6 (Kernel Boot Parameters) of the i.MX 6Dual/6Quad SABRE-SD Linux Release Notes.

The parameter would be ip and you can set it to ip = dhcp.

I hope this information helps!

Regards,

0 件の賞賛
返信