How to boot linux with multi image boot with an initrd packed with it

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to boot linux with multi image boot with an initrd packed with it

4,942 次查看
kevin_chaves
Contributor III

I'm having a hard time getting an initrd to work nicely with a multi image boot. I'm using an imx6 quad with 1 gb or ram. Our starting address with it is 0x80000000.

So I have an issue with using the normal cpio image built into the kernel as an initramfs. My problem is that we have proprietary modules so it becomes a circular dependency in the tool we got from timesys. To be able to build the cpio in the kernel image I need to build the modules first, which require the kernel to be built, which needs the mudels... So I've opted for a single file with multiple images built into it. But I'm having a hard time finding any decent documentation with this.

I've noticed that the kernel load address is the same as the ramdisk which I'm not sure if this is a problem. I do have both images separate, but I'm not entirely sure where to load cpio image separate. It seems like that could be easier since then I could just use bootm {kerneladdress} {cpioaddress} ?

## Booting kernel from Legacy Image at 80800000 ...

   Image Name:   Linux-3.0.35

   Image Type:   ARM Linux Multi-File Image (uncompressed)

   Data Size:    61927702 Bytes = 59.1 MiB

   Load Address: 80008000

   Entry Point:  80008000

   Contents:

      Image 0: 3581868 Bytes = 3.4 MiB

      Image 1: 58345822 Bytes = 55.6 MiB

   Verifying Checksum ... OK

## Loading init Ramdisk from multi component Legacy Image at 80800000 ...

## Flattened Device Tree from multi component Image at 80800000

   Loading Multi-File Image ... OK

The kernel arguments I used I pulled from the only example of the multi image I could find.

] Kernel command line: console=ttymxc1,115200 consoleblank=0 root=/dev/ram0 rw initrd=80800000 rootfstype=cpio

...

[    1.152419] Unpacking initramfs...

[    1.155854] Initramfs unpacking failed: junk in compressed archive

[    1.173722] Freeing initrd memory: 56980K

...

I'm not sure if i needed this but I added some config options to my kernel

CONFIG_BLK_DEV_INITRD=y

CONFIG_INITRAMFS_SOURCE=""

CONFIG_RD_GZIP=y

# CONFIG_RD_BZIP2 is not set

# CONFIG_RD_LZMA is not set

# CONFIG_RD_XZ is not set

# CONFIG_RD_LZO is not set

0 项奖励
回复
4 回复数

2,699 次查看
kevin_chaves
Contributor III

I found some mistakes apparently, someone mentioned i don't really need more than the console arguments.

console=ttymxc1,115200 consoleblank=0

and if i do use them rootfstype=ramfs

Also I didn't have the ram disk block driver enabled in the kernel.

[1.203461] Trying to unpack rootfs image as initramfs...
[1.209196] rootfs image is not initramfs (junk in compressed archive); looks like an initrd
[1.229656] Freeing initrd memory: 3080K

66] RAMDISK: Couldn't find valid RAM disk image starting at 0.

I also removed most of the user space libraries out, its more reasonable at 6.9 mb. Just enough to use busy box, and custom modules.

0 项奖励
回复

2,699 次查看
YixingKong
Senior Contributor IV

Kevin

Are you fine with the issue or do you need further help?

Thanks,

Yixing

0 项奖励
回复

2,699 次查看
kevin_chaves
Contributor III

I believe so, there wasn't any real reason why most of my options didn't work. I ended up basically with an uncompressed cpio image since none of the compression was working, the multipart image I couldn't get working at all so I just loaded the cpio image separately.

Due to the build system, the initramfs which had the least issues I couldn't use because of dependancies on some kernel modules and another oddity in which the order of the build seemed wrong.

0 项奖励
回复

2,699 次查看
YixingKong
Senior Contributor IV

Kevin

If I am correct, you are fine now and the issue can be closed.

Thanks,

Yixing

0 项奖励
回复