How to boot into a luks encrypted rootfs partition from initramfs on i.MX6ULZ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to boot into a luks encrypted rootfs partition from initramfs on i.MX6ULZ?

14,592 次查看
skwang6272
Contributor II

Hi everyone, 

I am trying to do disk encryption on i.MX6UL. The device is USB armory II. It has DCP and no CAAM.

This is my plan:

1、Two partitions. One for /boot, one for rootfs. Bootloader and kernel are stored in /boot and they are in plain text. The rootfs is encrypted by LUKS(DM-crpty).

2、Configure initramfs in the kernel. During the boot process, decrypt the encrypted rootfs and mount the root directory automatically.

3、LUKS uses file as key. At the same time this key file is encrypted with DCP.

Here is my question:

1、How to install the system on an already partitioned SD card?How to configure the encrypted file system?

2、How to configure initramfs to encrypt and load rootfs automatically?

I am just new to embedded development. Any suggestions, documentation and tutorials are welcome.

I have searched for similar issues

How to boot into a luks encrypted rootfs partition from initramfs on imx6 quad?

The document "Root filesystem encryption using DM-Crypt"  looks useful but I don't have permission to access it.

Thanks!

标签 (1)
28 回复数

6,038 次查看
aadebayo
Contributor I

Dear Mr. Yuri
I also working on rootfs encryption for IMX6, if you could please also provide me with a copy of the "Root filesystem encryption using DM-Crypt" document I would appreciate ie.
Best regards,

Adeola 

0 项奖励
回复

11,259 次查看
MikeAtMT
Contributor I

+1 looking for "Root filesystem encryption using DM-Crypt" - I've worked on this many years ago, but need to refresh my memory. Thank you!

12,221 次查看
r1cebank
Contributor II

Hi,

I am not sure if you already figured this out, but recently I've modified the USB Armory's image builder script to support the encrypted rootfs you mentioned.

https://github.com/r1cebank/usbarmory-debian-base_image

Hope this helps.

12,742 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following app note (assuming encrypted boot of U-boot and kernel).
"i.MX Encrypted Storage Using CAAM Secure Keys"
 
https://www.nxp.com/docs/en/application-note/AN12714.pdf

Regards,

Yuri.

0 项奖励
回复

12,742 次查看
skwang6272
Contributor II

Hi,

Thanks a lot!

But I have seen this doc. And I have no CAAM, only DCP. Are threy same?

0 项奖励
回复

12,742 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  If i.MX processor does not have CAAM - only software based DM-crypt

may be applied.

Regards,

Yuri.

0 项奖励
回复

10,363 次查看
adde_ado
Contributor III

Hi Yuri,

Could you please send to me 

"Root filesystem encryption using DM-Crypt" document?

I'm working with Imx8mm and I have same issue.

Best regards,

Adde

0 项奖励
回复

12,742 次查看
skwang6272
Contributor II

Hi, 

Thank you for your reply. Could you show me any docs explain how to preform software based DM-crypt?

btw Why can't DCP do what CAAM does?

0 项奖励
回复

12,742 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Some material have been sent directly.

Regards,

Yuri.

0 项奖励
回复

9,339 次查看
arunkrishnank
Contributor I

Dear Yuri,

Is it possible to share the document to me. I am attempting rootfs encryption on a i.MX 6 ULL

0 项奖励
回复

11,899 次查看
andreamengalli
Contributor II

Hello Yuri,

I am working on encryption on i.MX8Mmini.

Could I have access to the document "Root filesystem encryption using DM-Crypt"?

Thanks in advance.

0 项奖励
回复

10,836 次查看
YoussefDALIL
Contributor I

Hello @Yuri ,

Could I have also access to the document "Root filesystem encryption using DM-Crypt"

I really need this document to work on my project please.

Waiting for your reply

Thanks

0 项奖励
回复

10,819 次查看
Yuri
NXP Employee
NXP Employee

@YoussefDALIL 
Hello,

In addition to AN12714 (i.MX Encrypted Storage Using CAAM Secure Keys) use
section 10.5 (Disk encryption acceleration) of i.MX Linux User's Guide.


https://www.nxp.com/webapp/Download?colCode=AN12714

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

 For specific customer's cases (OS releases) NXP Pro Support may be involved.

Regards,
Yuri.

0 项奖励
回复

5,438 次查看
beestarbush
Contributor I

Hello,

I have the AN12714 and IMX Linux User Guide (IMXLUG_6.6.23_2.0.0) but would like to have a look into "Root filesystem encryption using DM-Crypt". Could you provide me this?

0 项奖励
回复

11,895 次查看
Yuri
NXP Employee
NXP Employee
0 项奖励
回复

11,378 次查看
parthitce
Contributor III

@YuriCould you please share the documents for dm-crypt to do with imx6ULL/imx6ULZ?

Thanks,

Parthiban N

11,371 次查看
Yuri
NXP Employee
NXP Employee

@parthitce 
Hello,

  I've sent You the file.

Regards,
Yuri.

0 项奖励
回复

4,942 次查看
kiranc
Contributor I

Hello Yuri,

I am also working on encryption.

Could I have access to the document "Root filesystem encryption using DM-Crypt"?

Thanks,

0 项奖励
回复

12,078 次查看
kmaincent
Contributor I

Hello Yuri,

I am also working on encryption.

Could I have access to the document "Root filesystem encryption using DM-Crypt"?

Thanks,

0 项奖励
回复

12,064 次查看
Yuri
NXP Employee
NXP Employee

@kmaincent 
Hello,

  I've sent You some comments.

Regards,
Yuri.

标记 (1)
0 项奖励
回复