How to avoid blank screen after splashscreen?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to avoid blank screen after splashscreen?

1,650 Views
paolosantini
Contributor III

When  I boot up my DART 6UL base on IMX.6ul, there're three different splashscreens (u-boot, kernel, and filesystem), after that  for few seconds, my lcd touchscreen changes in text mode, before to start my app.

How can I do to remove this text appearance and start my app immediately?

Labels (3)
0 Kudos
Reply
1 Reply

1,497 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, you are not using a board sold by NXP, there is not much we can help you. I recommend you to go with variscite, they could help you better with this problem.

However, if you are using Yocto as OS, there is a file called init.rc that is located on the /etc folder, on that file you can add processes that will be performed during the initialization of the board. You can add the initialization of your app on that file. Hope this can help you.

I apologize for the inconveniences this could give you.

Best regards,

Diego.

0 Kudos
Reply