How to add support for 16 bit bayer in iMX8M 

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to add support for 16 bit bayer in iMX8M 

2,133 次查看
ashwanthselvam
Contributor III

What are the changes that has to be done in CSI and capture driver for adding 16 bit bayer support?gogoer

标签 (1)
0 项奖励
回复
3 回复数

1,751 次查看
b36401
NXP Employee
NXP Employee

Unfortunately i.MX8M natively does not support more than 8 bits per component on video input.
So you can process debayering only software way in case of 16 bit.
However we have no such examples. Sorry for the inconvenience.

0 项奖励
回复

1,751 次查看
ashwanthselvam
Contributor III

Hi,

I don't need support on the debayering but on the input side.

I am making the changes as per datasheet for bayer 16 bit. But I am facing base address switching Change Err

I just want to know the changes required on the input side, So I can overcome that issue.

The CSI module accepts 8-bit, 10-bit or 16-bit data from the sensor by configuring
PIXEL_BIT bit in CSI Control Register 1 (CSICR1) and TWO_8BIT_SENSOR bit in
CSI Control Register3 (CSICR3).

0 项奖励
回复

1,751 次查看
b36401
NXP Employee
NXP Employee

With unsupported data types and the Rx Controller configured for single pixel mode, the raw packet data (including the header but minus the CRC) is contained on data_out[7:0].

0 项奖励
回复