Hi,
I don't need support on the debayering but on the input side.
I am making the changes as per datasheet for bayer 16 bit. But I am facing base address switching Change Err
I just want to know the changes required on the input side, So I can overcome that issue.
The CSI module accepts 8-bit, 10-bit or 16-bit data from the sensor by configuring
PIXEL_BIT bit in CSI Control Register 1 (CSICR1) and TWO_8BIT_SENSOR bit in
CSI Control Register3 (CSICR3).