How to add h264parse and overlay plugins to gst-1.0 in yocto ??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to add h264parse and overlay plugins to gst-1.0 in yocto ??

2,822 次查看
subodh
Contributor III

Hi ,

I want  add h264parse and overlay plugins to gstreamer 1.0.

Following in my query

https://www.mail-archive.com/meta-freescale@yoctoproject.org/msg10924.html

Please guide me.

LeonardoSandovalGonzalez OtavioSalvador DaianeAngolini

标签 (4)
4 回复数

2,252 次查看
daiane_angolini
NXP Employee
NXP Employee
0 项奖励
回复

2,252 次查看
subodh
Contributor III

I have setup the build as per following link

http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/README?h=imx-3.10.31-1.1.0_beta

The mentioned folder for recipes only contains jlive and no pakagegroups folder.

How do I get the updates to my system ?

Or is their any set of steps I can follow to build these manually ?

Thanks

0 项奖励
回复

2,252 次查看
daiane_angolini
NXP Employee
NXP Employee

The file I shared can be downloaded in your tree and modified.

It´s only an example.

If you want to try FSL Community BSP, please, FSL Community BSP

And it would be good if you could read the release notes: FSL Community BSP

2,252 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Thank you for the help, Daiane!

0 项奖励
回复