How to add a new NAND Flash support in iMX WinCE BSP -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add a new NAND Flash support in iMX WinCE BSP -blog archive

7,504 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

To support a new NAND in WinCE BSP, you need add the NAND information into file "WINCE600\PLATFORM\COMMON\SRC\SOC\COMMON_FSL_V2_PDK1_9\NAND\INC\NANDTYPES.h".

The "NANDCode" line is hard to get from NAND datasheet, you can also print it ot from driver code, file "WINCE600\PLATFORM\COMMON\SRC\SOC\COMMON_FSL_V2_PDK1_9\NAND\FMDCOMMON\BIG_SECTOR_INTERLEAVE\fmd.cpp"
Function FMD_Init(), you can add the debug message as followed:

... ...
           CSPNAND_Reset(i);
           FullCode = CSPNAND_ReadID(i);
           //only support multi-nand with same type
           //only support multi-nand connected continously
RETAILMSG(TRUE, (TEXT("NAND FullCode = 0x%x\r\n"), FullCode));  // Print out the current NAND flash code
           for(j = 0; j < sizeof(ChipInfo)/sizeof(ChipInfo[0]); j++)

... ...

 

An example to support the NAND NAND01GW3B2CNb

    //NAND01GW3B2CNb
    {
        {NAND, 1024, 2048 * 64, 64, 2048},          //FlashInfo   fi;
        {0x20, 0xF1, 0x00, 0x1d},                   //BYTE        NANDCode[NANDID_LENGTH]
        3,                                          //BYTE        NumBlockCycles
        5,                                          //BYTE        ChipAddrCycleNum
        8,                                          //BYTE        DataWidth
        1,                                          //BYTE        BBMarkNum
        {0},                                        //BYTE        BBMarkPage
        6,                                          //BYTE        StatusBusyBit
        0,                                          //BYTE        StatusErrorBit
        64,                                         //WORD        SpareDataLength
        0x70,                                       //BYTE        CmdReadStatus
        0x00,                                       //BYTE        CmdRead1
        0x30,                                       //BYTE        CmdRead2
        0x90,                                       //BYTE        CmdReadId
        0xff,                                       //BYTE        CmdReset
        0x80,                                       //BYTE        CmdWrite1
        0x10,                                       //BYTE        CmdWrite2
        0x60,                                       //BYTE        CmdErase1
        0xD0,                                       //BYTE        CmdErase2
        {30, 20, 25, 6}                             //NANDTiming  timings
    },

Tags (1)
0 Kudos
Reply
21 Replies

5,275 Views
Radist
Contributor II

with this parameters all test's was passed ok. Its interesting, but Freescale BSP write 2 copies of EBOOT to the NAND. 6 block is needed for 1 copy at 2k page size 

0 Kudos
Reply

5,275 Views
KeshavaGN
Contributor V

Hi Radist ,

Please help me to solve this issue: iMX6Q NAND Boot issue in WinCE

Thanks.

With regards,

Keshava G N

0 Kudos
Reply

5,275 Views
Radist
Contributor II

Hi Keshave G N!

i was out of internet few weeks :smileyhappy: Will read your questions and contact

you soon.

Keshava G N пишет:

>

Freescale Community <https://community.freescale.com/index.jspa>

<https://community.freescale.com/index.jspa>

>

You have been mentioned

by Keshava G N <https://community.freescale.com/people/KeshavaGN> /in

Re: How to add a new NAND Flash support in iMX WinCE BSP -blog archive

in Freescale Community/ - View Keshava G N's reference to you

<https://community.freescale.com/message/313359#313359>

0 Kudos
Reply

5,275 Views
KeshavaGN
Contributor V

Thank you Makovetskyi!

With regards,

Keshava G N

Member - Technical (Software)

From: Sergii Makovetskyi

Sent: Monday, January 28, 2013 12:53 AM

To: Keshava G N

Subject: Re: - How to add a new NAND Flash support in iMX WinCE BSP -blog archive

How to add a new NAND Flash support in iMX WinCE BSP -blog archive

created by Sergii Makovetskyi in i.MX Community - View the full discussion

0 Kudos
Reply

5,275 Views
Radist
Contributor II
Offset (in blocks)Block countBlock nameOffset variable name in BSPDescription
04BCBIMAGE_BOOT_NCB_NAND_OFFSETBoot Control Block
44BBTIMAGE_BBT_NAND_OFFSETBad Block Table
82DBBTIMAGE_BOOT_DBBT_NAND_BLOCKSBad block table used by ROM
1012EBOOT IMAGE 1IMAGE_BOOT_BOOTIMAGE_NAND_BLOCKSEboot image, 2 copy (6 * 2) NOTE: EBOOT assumes these NAND regions are block-aligned
SPLASH SCREEN 1
EBOOT IMAGE 2
SPLASH SCREEN 2
221
IMAGE_BOOT_BOOTCFG_NAND_BLOCKSBoot configuration
231
IMAGE_BOOT_UUID_NAND_BLOCKSUUID
24XXX (32MB)NKIMAGEIMAGE_BOOT_NKIMAGE_NAND_OFFSETOS WinCE Kernel 32MB
XXXLast blockFFS
Flash File System
IMAGE_BOOT_NANDDEV_RESERVED_SIZE (for NAND with 2k page, 64 pages in block) = 24*2048*64 + 32*1024*1024 = 35*1024*1024
IMAGE_BOOT_NANDDEV_RESERVED_SIZE (for NAND with 4k page, 128 pages in block) = 24*4096*128 + 32*1024*1024 =44*1024*1024
0 Kudos
Reply

5,274 Views
Radist
Contributor II

Hi, 

yes, exactly. And it work ok when i am using resistors for boot mode configuration. Than i remove boot mode resistors, set pull down resistor to LCD_RS  (enable boot from source, that configured by  OTP fuses). And tried to boot from NAND 1Gbit? but... xldr started ok and eboot have crashed. 

Than i change  IMAGE_BOOT_BOOTIMAGE_NAND_BLOCKS back to 512. And its start work ok.

Do you know why it is work in that way? have you tried too boot from OTP-configured boot source? 

0 Kudos
Reply

5,275 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

There is a BSP bug in file "image_cfg.h", it defines IMAGE_BOOT_BOOTIMAGE_NAND_BLOCKS  (512)

That means the EBoot reserved 512 blocks NAND size, for 128KB block size NAND, it is 64MB, it is not reasonable, and this will cause system hang up when we used the small size NAND.

The code should be updated as followed:

#define IMAGE_BOOT_BOOTIMAGE_NAND_BLOCKS      (8)

0 Kudos
Reply

5,275 Views
Radist
Contributor II

Do you know, what is the minimum size for the IMAGE_BOOT_NANDDEV_RESERVED_SIZE ?

i just sent it to 32M and its work now. But i think its too small...

0 Kudos
Reply

5,275 Views
Radist
Contributor II

result is the same:

11876 PID:400002 TID:ea0002 reset GPMI module

  11876 PID:400002 TID:ea0002 --SMA DEBUG: NAND FullCode = 0x9580f12c

  11904 PID:400002 TID:ea0002 --SMA DEBUG: NAND FullCode = 0x0

  11904 PID:400002 TID:ea0002 NumberOfChip=1

  11904 PID:400002 TID:ea0002 ECC_ConfigLayout

  11941 PID:400002 TID:ea0002 --SMA debug: BSP_GetNANDImageCfg IMAGE_BOOT_NANDDEV_RESERVED_SIZE =  0x4600000

  11941 PID:400002 TID:ea0002 --SMA debug: BSP_GetNANDImageCfg IMAGE_BOOT_NANDDEV_RESERVED_SIZE =  0x4600000

  11941 PID:400002 TID:ea0002 INFO: Set NAND flash blocks [0x0 ~ 0x22f] as reserved.

  11941 PID:400002 TID:ea0002 --SMA debug1: dwNandSize =  0x4600000

  11941 PID:400002 TID:ea0002 --SMA debug1: dwBytesPerBlock =  0x20000

  12001 PID:400002 TID:ea0002 ERROR: C:\WINCE600\PLATFORM\COMMON\SRC\SOC\MX28_FSL_V2_PDK1_9\MEDIA\NAND\CORE\.\cspnand.c line 505:

  12001 PID:400002 TID:ea0002 FMD_Deinit: FMD Driver is unloading (c095d8a0)

NAND code is correct, chip is 1Gbit. With 8G and 4G everything is ok...

0 Kudos
Reply

5,274 Views
Radist
Contributor II

ok, thanks, i already made the same steps. Only 1 difference -i set IMAGE_BOOT_NANDDEV_RESERVED_SIZE to 64M, you have set it to 70M. Now i am rebuilding my OS with 70M.

0 Kudos
Reply

5,275 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

NAND support for iMX28 (BSP version: WCE600_10.08.02_SDK.msi)

The detail steps for me to support the 128MB SLC NAND NAND01GW3B2CNb:

 

1. Catalog -> iMX28-EVK-PDK1_9-Monility -> Third Party -> BSP -> Freescale i.MX28 EVK PDK1_9: ARMV4I -> Device Drivers -> SD Controller
remove "SSP2 SDHC"

2. Catalog -> iMX28-EVK-PDK1_9-Monility -> Device Drivers -> Storage Devices -> MSFlash Drivers
select "Flash MDD"

3. Visual Studio 2005 menu: Project -> iMX28-EVK-PDK1_9-Mobility Property ...
Configuration Properties -> Environment
remove "imgsdmmc";  add "imgnand" and set value to 1.

4. BSP code, modify file “WINCE600\PLATFORM\COMMON\SRC\SOC\COMMON_FSL_V2_PDK1_9\NAND\INC\NANDTYPES.h”, data structure NandChipInfo ChipInfo[], added the followed codes:
    //NAND01GW3B2CNb
    {
        {NAND, 1024, 2048 * 64, 64, 2048},          //FlashInfo   fi;
        {0x20, 0xF1, 0x00, 0x1d},                   //BYTE        NANDCode[NANDID_LENGTH]
        3,                                          //BYTE        NumBlockCycles
        5,                                          //BYTE        ChipAddrCycleNum
        8,                                          //BYTE        DataWidth
        1,                                          //BYTE        BBMarkNum
        {0},                                        //BYTE        BBMarkPage
        6,                                          //BYTE        StatusBusyBit
        0,                                          //BYTE        StatusErrorBit
        64,                                         //WORD        SpareDataLength
        0x70,                                       //BYTE        CmdReadStatus
        0x00,                                       //BYTE        CmdRead1
        0x30,                                       //BYTE        CmdRead2
        0x90,                                       //BYTE        CmdReadId
        0xff,                                       //BYTE        CmdReset
        0x80,                                       //BYTE        CmdWrite1
        0x10,                                       //BYTE        CmdWrite2
        0x60,                                       //BYTE        CmdErase1
        0xD0,                                       //BYTE        CmdErase2
        {30, 20, 25, 6}                             //NANDTiming  timings
    },


5. BSP code, modify file "WINCE600\PLATFORM\iMX28-EVK-PDK1_9\SRC\INC\image_cfg.h”, modify IMAGE_BOOT_NANDDEV_RESERVED_SIZE as followed:
    #define IMAGE_BOOT_NANDDEV_RESERVED_SIZE    (DWORD)((DWORD)(70 * 1024 * 1024))

0 Kudos
Reply

5,275 Views
Radist
Contributor II

I mean next things, Did you had error "ERROR: C:\WINCE600\PLATFORM\COMMON\SRC\SOC\MX28_FSL_V2_PDK1_9\MEDIA\NAND\CORE\.\cspnand.c line 505: 11877 PID:400002 TID:ea0002 FMD_Deinit: FMD Driver is unloading (c095d8a0)" before changing IMAGE_BOOT_NANDDEV_RESERVED_SIZE    with right NANDcode.

My NAND code is right, because eboot can see this chip and able to format it.

0 Kudos
Reply

5,275 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Yes, I see such error when I set NANDCode to wrong.

0 Kudos
Reply

5,275 Views
Radist
Contributor II

Did you had the same error that i have? before you have changed this variable

0 Kudos
Reply

5,274 Views
Radist
Contributor II

yes, NAND ID is correct and i can see NAND from eboot. able to format it.

0 Kudos
Reply

5,275 Views
Radist
Contributor II

Yes, ofcourse i already made it. Strange situation. Small difference - i have tried to change variable to 64 or 128 MB, i did not tried to set 70. Will try to do it now. I am using SLC MT29F1G08ABADAW. Did you had the same error that i had? before you have changed this variable

0 Kudos
Reply

5,275 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Did you print out the NAND ID with the followed code?

RETAILMSG(TRUE, (TEXT("NAND FullCode = 0x%x\r\n"), FullCode));  // Print out the current NAND flash code

0 Kudos
Reply

5,275 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Yes I used the iMX28 EVK board, with the 128MB SLC NAND (NAND01GW3B2CNb), I think you need rebuild both the eboot and NK.

0 Kudos
Reply

5,275 Views
Radist
Contributor II

Hi! Thanks for the answer,

its interesting, but i also update this variable and its still not work. What kind of NAND are you using? Do you work with iMX28 ?

0 Kudos
Reply

5,274 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

To support a small NAND, the IMAGE_BOOT_NANDDEV_RESERVED_SIZE in image_cfg.h should be updated. For example, I had modified it to "#define IMAGE_BOOT_NANDDEV_RESERVED_SIZE    (DWORD)((DWORD)(70 * 1024 * 1024))" for a 128MB NAND, it works fine.

0 Kudos
Reply