Our software on Linux Desktop uses this GSTreamer v1.22.3 to achieve VA-API-based hardware-accelerated IP camera video decoding with just about 220ms delay using this pipeline:
rtspsrc location=rtsp://... protocols=tcp latency=100 buffer-mode=slave ! queue max-size-buffers=0 ! rtph264depay ! h264parse ! vah264dec compliance=3 ! glupload ! glcolorconvert ! qmlglsink
Meanwhile, to show RTSP stream on imx8mm this pipeline is used:
rtspsrc location=rtsp://... protocols=udp latency=200 buffer-mode=slave ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! h264parse ! queue max-size-buffers=0 ! imxvpudec_h264 ! queue max-size-buffers=0 ! glupload ! qmlglsink sync=1
It seems that I need to use latency=200 in order to keep stable 25fps. If I reduce rtspsrc latency to same 100 as on Desktop, I get "wobbling", unstable and low framerate, some times dropping to 11fps for example. And if I keep 200ms latency, final real delay (measured by screencaping running timer, etc) is near 400ms, which is rather high for our use case.
I have same FPS issues even if I use "raw" glimagesink, launched via gst-launch-1.0 via terminal.
Maybe there are some "tricks" what I don't know that would help to display RTSP streames with lower latency, but with still stable 25fps video in i.MX8M Mini machines?
Thanks!
It seems there's sort of regression in GStreamer itself since 1.22.2 - I actually no longer get ~220ms on PC either: https://gitlab.freedesktop.org/gstreamer/gstreamer/-/issues/2702
I do get good performance in older 1.22.1 on PC, but I can't build it for NXP because of other bug (seems fixed in 1.22.3):
../src/ext/qt/gstqtglutility.cc:48:10: fatal error: gst/gl/viv-fb/gstgldisplay_viv_fb.h: No such file or directory
48 | #include <gst/gl/viv-fb/gstgldisplay_viv_fb.h>
Hello,
NXP don't have any latency measurement of this, because is relative you are measurement with the keyword = 200, but this is not real, it based on your connection and some fails that can be present in the line, I use tune=zerolatency and it does the trick for me (200ms latency).
Regards