How to access serial port from Android MM application ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to access serial port from Android MM application ?

10,283 Views
arindamroy
Contributor II

SE Policy prevents access of serial ports by android application (by default).

I added "allow" to untrusted_app.te

allow untrusted_app tty_device:chr_file rw_file_perms;

However, still the avc denial message comes up that untrusted_app not permitted to write to tty_device.

How can this be resolved ?

Labels (2)
0 Kudos
Reply
12 Replies

9,293 Views
bensonwu
Contributor III

arindamroy

I have struggled this issue for 2 days with the same symptom as yours...and finally, I solved this issue with SELINUX on.

============================= My Solution ========================================= 

  • First , try to search the "tty_device" in external/sepolicy/ folder ,then I found there is a command in device.te 

type tty_device, dev_type;

  • Try to modify the command as follows :

type tty_device, dev_type, mlstrustedobject;

  • Everything is back to normal.

All the above solution is coming from the ideas of the link: SELinux 添加一个权限 - 大大世界 - 简书 

However, I am not really uncertain why this action solved this issue... 

0 Kudos
Reply

9,293 Views
bensonwu
Contributor III

I have the same issue , too.  Did anybody have solution? 

0 Kudos
Reply

9,293 Views
diegoadrian
NXP Employee
NXP Employee

Probably I will need an apk that could work in the sabresd6q and make all the features that you need. It would be helpful if you can pass me an apk to test the problem.

Best Regards,

Diego.

0 Kudos
Reply

9,293 Views
chum
Contributor III

Hi Diego,

I'm new to android,

How to test imx6q sabre-sdb serial port with android apk?

i want to send some data to serial

if any sample apk is available please suggest me

thanks

0 Kudos
Reply

9,293 Views
diegoadrian
NXP Employee
NXP Employee

Hello Arindam,

Do you have any script regarding, or an App regarding to this issue?

I have successfully built the image, but I need to reproduce your error.

Best Regards,

Diego.

0 Kudos
Reply

9,293 Views
arindamroy
Contributor II

Hi Diego,

I am trying to access serial port (ttymxc1) from my app. A simple open followed by a read.

I do not have a separate test app. I believe a simple app which just opens and reads ttymxc1 or ttymxc2 will be sufficient to reproduce the issue.

If required, I can create one.

Regards,

Arindam

0 Kudos
Reply

9,293 Views
diegoadrian
NXP Employee
NXP Employee

Hello Arindam,

You can try to set this boot targets during the boot process.

setenv bootargs 'console=ttymxc2,115200 init=/init video=mxcfb0:dev=ldb,1024x768M@60,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.console=ttymxc2 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled no_console_suspend'

I haven't tested this configuration with an app. But I can write to the serial ports thought shell commands.

I hope this can solve your problem.

Best Regards,

Diego.

0 Kudos
Reply

9,293 Views
arindamroy
Contributor II

Hi Diego,

I do not want to disable SELINUX.

Regards,

Arindam Ghosh Roy

Principal Firmware Engineer | Renal Care Solutions

India Medtronic Pvt. Ltd.

Prestige Shantiniketan, Tower B, 11th Floor | Whitefield, Bangalore – 560048 | INDIA

Office +91 80 6715 7351 | Mobile + 91 70220 24759| Fax +91 80 6715 7498

arindam.g.roy@medtronic.com<mailto:arindam.g.roy@medtronic.com>

medtronic.com<http://www.medtronic.com/> | Facebook<https://www.facebook.com/Medtronic> | LinkedIn<https://www.linkedin.com/company/medtronic?trk=biz-companies-cym> | Twitter<https://twitter.com/Medtronic> | YouTube <https://www.youtube.com/user/MedtronicCorp>

LET’S TAKE HEALTHCARE

FURTHER, TOGETHER

0 Kudos
Reply

9,293 Views
diegoadrian
NXP Employee
NXP Employee

Hello Arindam,

I am trying to build the image with the new configurations. But I am getting some errors that I am trying to solve on the go.

I will notify you, If I can successfully build the image.

Best Regards,

Diego.

0 Kudos
Reply

9,293 Views
diegoadrian
NXP Employee
NXP Employee

Hello Arindam,

I found this web-page that can help you with your problem. I haven't tested the solution, but you can try it and see if it works.

Android* Security Customization with SEAndroid - CodeProject 

Best Regards,

Diego.

0 Kudos
Reply

9,293 Views
arindamroy
Contributor II

Hi Diego,

Thank you for the reply.

I did use the rule ( as specified in the link also ):

allow untrusted_app tty_device:chr_file rw_file_perms;

and ttymxc1 and ttymxc2 falls under the category tty_device.

I am using Sabre SDP and Android Marshmallow.

Could you reproduce in to the board ?

Regards,

Arindam

0 Kudos
Reply

9,293 Views
diegoadrian
NXP Employee
NXP Employee

Hello Arindam,

 

Thank you for writing.

 

I will try to reproduce this error, probably this process can take some time.

Best regards,

Diego.

0 Kudos
Reply