How to Flash Android 9 on IMX8 with 128G eMMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Flash Android 9 on IMX8 with 128G eMMC

16,395件の閲覧回数
weikeng-jimmy
Contributor III

Hi Sir,

My customer want to expand EMMC size from 32GB to 128GB. We modify and new a 128GB bpt file as below.

1.

{
"settings": {
"disk_size": "128 GiB",
"disk_alignment": 2097152,
"first_partition_offset": 8388608
},

2. Modify ~/ANDROID_CODEBASE/device/fsl/imx8m/rom5720_a1/BoardConfig.mk

# Support gpt
BOARD_BPT_INPUT_FILES += device/fsl/common/partition/device-partitions-13GB-ab.bpt
ADDITION_BPT_PARTITION = partition-table-7GB:device/fsl/common/partition/device-partitions-7GB-ab.bpt \
partition-table-128GB:device/fsl/common/partition/device-partitions-128GB-ab.bpt \
partition-table-28GB:device/fsl/common/partition/device-partitions-28GB-ab.bpt


We try to use uuu tool and get a fail when use download command.

./uuu_imx_android_flash.sh -f imx8mq -a -e -c 128


Please help to modify a "128GB dual-bootloader" .bpt file for 128G eMMC.

Thansk~

ラベル(2)
23 返答(返信)

1,693件の閲覧回数
lisztkao
Contributor II

Rename file partition-table-28GB.img to partition-table-128GB.img and flash image via uuu tool.

emmc_uuu.jpg

The storage in Setting application shown

emmc_storage.jpg

0 件の賞賛
返信

1,624件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Sorry for my last reply, I have confirmed and discussed with our expert team. Get feedback from them that if you are using the 128GB emmc, you steps is right at first, but you need to modify  the file device-partitions-128GB-ab.bpt add the

"disk_size": "119 GiB"

                                                                                                       

 

0 件の賞賛
返信

1,615件の閲覧回数
weikeng-jimmy
Contributor III

My customer modify partitions-128GB-ab.bpt and flash image via uuu tool , but it's still burn fail.

1.jpg

2.jpg3.jpg4.jpg

0 件の賞賛
返信