IMX6UL DDR3 Stress test failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL DDR3 Stress test failed

2,177 Views
ganesh_k
Contributor III

Hi team,

   Greetings of the day...

            We have a customized imx6ul board which is having the two RAM chips(MT41K512M8DA-107P) connected parallel and using one CS pin DRAM_CS0. got the NXP DDR test tool from your links. Below are the options selected while testing the stress through USB for customized board.

Target : IMX6UL       ARM Speed : 528MHz   

DDR Density : 1GB   DDR CS: 0   DDR Channel: 0

MR1 value: 0004      Start Freq: 350

DDR Freq: 400         End Freq: 400

 

Below are the logs for stress test:

****************************************************************************************************************************************

============================================
DDR Stress Test (3.0.0)
Build: Dec 14 2018, 14:13:14
NXP Semiconductors.
============================================

============================================
Chip ID
CHIP ID = i.MX6 UltraLite(0x64)
Internal Revision = TO1.2
============================================

============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00004860
SRC_SBMR2(0x020d801c) = 0x02000041
============================================

ARM Clock set to 528MHz

============================================
DDR configuration
DDR type is DDR3
Data width: 16, bank num: 8
Row size: 16, col size: 10
Chip select CSD0 is used
Density per chip select: 1024MB
============================================


DDR Stress Test Iteration 1
Current Temperature: 41
============================================

DDR Freq: 352 MHz
t0.1: data is addr test
Address of failure(step2): 0x80000000
Data was: 0x8500002a
But pattern should match address
Error: failed to run stress test!!!

**************************************************************************************************************************************

attached the inc file which is using for above test. please let me know where i am doing the mistake.

Thanks & Regards

Ganesh.K

Labels (3)
0 Kudos
7 Replies

1,955 Views
Ang_447
Contributor I

Hello, I am having the same problem.

Chip ID
CHIP ID = i.MX6 UltraLiteLite(0x65)
Internal Revision = TO1.1
============================================

============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00000000
SRC_SBMR2(0x020d801c) = 0x00000001
============================================

ARM Clock set to 528MHz

============================================
DDR configuration
DDR type is DDR3
Data width: 16, bank num: 8
Row size: 15, col size: 10
Chip select CSD0 is used
Density per chip select: 512MB
============================================


DDR Stress Test Iteration 1
Current Temperature: 47
============================================

DDR Freq: 148 MHz
t0.1: data is addr test
Address of failure(step2): 0x80000000
Data was: 0x98000000
But pattern should match address
Error: failed to run stress test!!!

0 Kudos

2,107 Views
Yuri
NXP Employee
NXP Employee

ganesh.k@phytecembedded.in 

Hello,

  I've sent You some comments directly.

Regards,

Yuri.

0 Kudos

2,107 Views
ganesh_k
Contributor III

hi sir,

      Sent a mail. Please check sir.

Thanks & Regards

Ganesh.K

0 Kudos

2,107 Views
ganesh_k
Contributor III

Dear sir,

         i have tested stress test with DDR density 512MB(default .inc file), successfully completed with 512MB, below is the log. But with 1GB its failing.

stress test with DDR density 512MB log(default .inc file):

*********************************************************************

============================================

DDR Stress Test (3.0.0)

Build: Dec 14 2018, 14:13:14

NXP Semiconductors.

============================================

============================================

Chip ID

CHIP ID = i.MX6 UltraLite(0x64)

Internal Revision = TO1.2

============================================

============================================

Boot Configuration

SRC_SBMR1(0x020d8004) = 0x00002042

SRC_SBMR2(0x020d801c) = 0x02000041

============================================

ARM Clock set to 528MHz

============================================

DDR configuration

DDR type is DDR3

Data width: 16, bank num: 8

Row size: 15, col size: 10

Chip select CSD0 is used

Density per chip select: 512MB

============================================

DDR Stress Test Iteration 1

Current Temperature: 43

============================================

DDR Freq: 352 MHz

t0.1: data is addr test

t0: memcpy11 SSN test

t1: memcpy8 SSN test

t2: byte-wise SSN test

t3: memcpy11 random pattern test

t4: IRAM_to_DDRv2 test

t5: IRAM_to_DDRv1 test

t6: read noise walking ones and zeros test

DDR Freq: 365 MHz

t0.1: data is addr test

t0: memcpy11 SSN test

t1: memcpy8 SSN test

t2: byte-wise SSN test

t3: memcpy11 random pattern test

t4: IRAM_to_DDRv2 test

t5: IRAM_to_DDRv1 test

t6: read noise walking ones and zeros test

DDR Freq: 380 MHz

t0.1: data is addr test

t0: memcpy11 SSN test

t1: memcpy8 SSN test

t2: byte-wise SSN test

t3: memcpy11 random pattern test

t4: IRAM_to_DDRv2 test

t5: IRAM_to_DDRv1 test

t6: read noise walking ones and zeros test

DDR Freq: 396 MHz

t0.1: data is addr test

t0: memcpy11 SSN test

t1: memcpy8 SSN test

t2: byte-wise SSN test

t3: memcpy11 random pattern test

t4: IRAM_to_DDRv2 test

t5: IRAM_to_DDRv1 test

t6: read noise walking ones and zeros test

Success: DDR Stress test completed!!!

Please provide the 1GB density .inc file. Thank you

0 Kudos

2,107 Views
Yuri
NXP Employee
NXP Employee

Hello,

  please try the following:

pastedImage_1.png

Regards,

Yuri.

0 Kudos

2,107 Views
ganesh_k
Contributor III

hi, thank you for your reply.. but as from above file, the memory typ is DDR3-1866 is not available in excel sheet.
please provide the DDR3-1866 related excel sheet which is having this option.

Thanks & Regards

Ganesh.K

0 Kudos

2,105 Views
Yuri
NXP Employee
NXP Employee

@ganesh_k 

Hello,

   The i.MX 6UL supports DRAM up to 400 MHz:
LP-DDR2-800, DDR3-800 and LV-DDR3-800

It does not support DDR3-1866, so use timings for DDR3-800.

Regards,
Yuri.

 

0 Kudos