How to Encrypt Root Filesystem in Yocto build Environment?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Encrypt Root Filesystem in Yocto build Environment?

7,007件の閲覧回数
trongthinh
Contributor IV

I followed the https://community.nxp.com/docs/DOC-342300 to encrypt my root filesystem. The document is so good. I am wondering if the step 3.6 in the document is done automatically in Yocto build environment. I would like to create a sdcard image that was already encrypted. 

ラベル(3)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

4,025件の閲覧回数
Massimo1980
Contributor I

Good morning and sorry for reply on a dated post.

Is it possible to have access to this document: https://community.nxp.com/docs/DOC-342300

Thanks in advance for your support

0 件の賞賛
返信

6,308件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately it is not done in our default Yocto, that came with Linux BSP, but this does not mean that you can make the Recipe, to add this step in Yocto Build Enviroment, you can follow the Yocto Training that we have available in the i.MX Training‌ sub-space.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信