How to Encrypt Root Filesystem in Yocto build Environment?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to Encrypt Root Filesystem in Yocto build Environment?

7,069 次查看
trongthinh
Contributor IV

I followed the https://community.nxp.com/docs/DOC-342300 to encrypt my root filesystem. The document is so good. I am wondering if the step 3.6 in the document is done automatically in Yocto build environment. I would like to create a sdcard image that was already encrypted. 

标签 (3)
标记 (2)
0 项奖励
回复
2 回复数

4,087 次查看
Massimo1980
Contributor I

Good morning and sorry for reply on a dated post.

Is it possible to have access to this document: https://community.nxp.com/docs/DOC-342300

Thanks in advance for your support

0 项奖励
回复

6,370 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately it is not done in our default Yocto, that came with Linux BSP, but this does not mean that you can make the Recipe, to add this step in Yocto Build Enviroment, you can follow the Yocto Training that we have available in the i.MX Training‌ sub-space.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复