How to Enable Secure boot in Imx8m?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Enable Secure boot in Imx8m?

ソリューションへジャンプ
4,560件の閲覧回数
ravindrajinka88
Contributor I

Hi, As an embedded engineer im much familier with Microcotroller, but im new to the imx (processor). currently i'm working with imx8m with Yocto. Here im having the problem in enabling secure boot in imx8m. To enable secure boot I'm referring the following links please let me know which is correct and also please let me know anything that i missed to refer.

link-1: mx8m_mx8mm_secure_boot.txt\guides\habv4\imx\doc - uboot-imx - i.MX U-Boot 

link-2: mx8_mx8x_secure_boot.txt\guides\ahab\imx\doc - uboot-imx - i.MX U-Boot 

Thanks,

Ravindra

0 件の賞賛
返信
1 解決策
4,334件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Use the following resource:

mx8m_mx8mm_secure_boot.txt\guides\habv4\imx\doc - uboot-imx - i.MX U-Boot 

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,335件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Use the following resource:

mx8m_mx8mm_secure_boot.txt\guides\habv4\imx\doc - uboot-imx - i.MX U-Boot 

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信