How much is the power consumption for RTC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How much is the power consumption for RTC?

1,402 Views
jacopoagostini
Contributor I

Hi, I wanted to know how the i.MX6UL handles the RTC. From the datasheet I seem to have understood that the RTC power consumption to be on is in the order of hundred of uA. In my PCB there is no space for a coin cell so I want to use a supercap to supply the RTC even when all system is off. The problem is that in this case the duration of the supercap is much lower than a coin cell because of the elevated RTC power consumption; so I want to ask if the RTC power consumption is really so excessive that I'm not allowed to use a Supercap.

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,186 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jacopo Agostini,

The RTC power consumption on the datasheet is correct and furthermore is a typical value, not the maximum possible RTC power consumption, which means it may be higher than that.

My apologies for the inconvenience.

Regards,

0 Kudos
Reply