How many gstreamer pipelines on imx8mm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How many gstreamer pipelines on imx8mm

994件の閲覧回数
matt67
Contributor III

Hello,

How many gstreamer pipelines could run in parallel in order to decode/re-encode H264 video streams.

My usecases are to decode 4 FHD (1920x1080) RSTP video source and re-encode to :

HD (720x1080) or FWVGA (480x854) depending on user setting.

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

988件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Matthieu 

 

>How many gstreamer pipelines could run in parallel in order to decode/re-encode H264 video streams

 

from hardware there are no limitation, limitation only from internal buses bandwidth.

So guaranteed performance is 1080p60, but with less fps/resolutions there may be more vpu instances

for example two 1080p30.

 

Best regards
igor

0 件の賞賛
返信