How many gstreamer pipelines on imx8mm

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How many gstreamer pipelines on imx8mm

1,075 次查看
matt67
Contributor III

Hello,

How many gstreamer pipelines could run in parallel in order to decode/re-encode H264 video streams.

My usecases are to decode 4 FHD (1920x1080) RSTP video source and re-encode to :

HD (720x1080) or FWVGA (480x854) depending on user setting.

 

Thanks

标签 (1)
0 项奖励
回复
1 回复

1,069 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Matthieu 

 

>How many gstreamer pipelines could run in parallel in order to decode/re-encode H264 video streams

 

from hardware there are no limitation, limitation only from internal buses bandwidth.

So guaranteed performance is 1080p60, but with less fps/resolutions there may be more vpu instances

for example two 1080p30.

 

Best regards
igor

0 项奖励
回复