How install data on integrity protected partitions during production using i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How install data on integrity protected partitions during production using i.MX6

1,224 Views
ufechner
Contributor I

When installing a new board support package from SD card
on the emmc of our board the following steps happen:
1. create a random key
2. encrypt it
3. store it on both the boot boot partition
4. decrypt the key and store it in RAM
5. we format the app end the home partition using the key from RAM
and the command "integritysetup format"
5. we open the app end the home partition using the key from RAM
and the command "integritysetup open" and copy the data from SD
card to eMMC
6. we close the app and the home partition

When we later boot from eMMC, the key is loaded and decrypted and the protected partitions are mounted.

The question is, when can we burn the fuses, in particular the "secure boot" fuse such that the unique, per device key is used for integrity protection?

If we do that before encrypting the key using the command "caam_tool enc", will the caam tool detect that the device is a secure device? I think it will not, because the device only becomes a secure device after power cycling.

So how can I create a secure device AND use per-device key for integrity protection without having to power cycle the device twice during the installation process?

The web page https://github.com/f-secure-foundry/caam-keyblob/ says:
"The secure operation of the CAAM and SNVS, in production deployments, should always be paired with Secure Boot activation."

Does this always requires an addition power cycling of the board before installing data on the secure partition?

Best regards:

Uwe Fechner

Tags (3)
0 Kudos
Reply
1 Reply

1,184 Views
igorpadykov
NXP Employee
NXP Employee

Hi Uwe

 

from team:

------------

Yes. Secure boot need a new power cycle to enable. CAAM key blob only can be decapsulated in the same life cycle as it is created. So additional power cycle is need.

------------

 

Best regards
igor

0 Kudos
Reply