How does sema4 use in linux applicaiton

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How does sema4 use in linux applicaiton

1,730件の閲覧回数
jingyangxie
Contributor V

I want to use sema4 to perform mutually exclusive operation between a9 and m4 applications, how can I achieve it, especially on A9 aside

ラベル(1)
0 件の賞賛
返信
1 返信

1,684件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jingyang

one can refer to https://community.nxp.com/thread/384413 

also additional document was sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------