How do I read and write fpga through EIM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I read and write fpga through EIM?

1,486 Views
martin_wilson
Contributor I

I 've now configured the EIM bus.  Is there an error? How do i read and write fpga through EIM?

static struct mtd_partition mxc_nor_partitions[] = {
{
.name = "FPGA.EIM",
.offset = 0,
.size = 0x00080000,
},
};
static struct resource nor_flash_resource = {
.start = CS0_BASE_ADDR,
.end = CS0_BASE_ADDR + 0x02000000 - 1,
.flags = IORESOURCE_MEM,
};

static struct physmap_flash_data nor_flash_data = {
.probe_type = "cfi_probe",
.width = 2,
.parts = mxc_nor_partitions,
.nr_parts = ARRAY_SIZE(mxc_nor_partitions),
};

static struct platform_device physmap_flash_device = {
.name = "physmap-flash",
.id = 0,
.dev = {
.platform_data = &nor_flash_data,
},
.resource = &nor_flash_resource,
.num_resources = 1,
};
/* eim */
static void mx6q_setup_eim_cs(void)
{
void __iomem *ram_reg = MX6_IO_ADDRESS(WEIM_BASE_ADDR);
void __iomem *ccm_reg = MX6_IO_ADDRESS(CCM_BASE_ADDR);
unsigned int reg;
struct clk *clk;
u32 rate;

/* CLKCTL_CCGR6: Set emi_slow_clock to be on in all modes */
reg = readl(ccm_reg + 0x80);
reg |= 0x00000C00;
writel(reg, ccm_reg + 0x80);

clk = clk_get(NULL, "emi_slow_clk");
if (IS_ERR(clk))
printk(KERN_ERR "emi_slow_clk not found\n");

rate = clk_get_rate(clk);
if (rate != 132000000)
printk(KERN_ERR "Warning: emi_slow_clk not set to 132 MHz!"
" WEIM NOR timing may be incorrect!\n");

writel(0x403304b1, ram_reg);
writel(0x0, ram_reg + 0x4);

writel(0x0f010000, ram_reg + 0x8);
writel(0x00000008, ram_reg + 0xc);

writel(0x0f040040, ram_reg + 0x10);
writel(0x00000000, ram_reg + 0x14);

writel(0x00000000, ram_reg + 0x90);
}

Labels (2)
0 Kudos
Reply
1 Reply

1,296 Views
igorpadykov
NXP Employee
NXP Employee

Hi

one can look at commands used by mfg tool (in ucl2.xml)

https://www.nxp.com/webapp/Download?colCode=IMX_L4.1.15_2.1.0_MFG_TOOL&appType=license&location=null... 

use for example mfgtool2-yocto-mx-sabreauto-weim-nor-cpu3.vbs script.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply