How do I find a replacement URL for Aurora?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I find a replacement URL for Aurora?

ソリューションへジャンプ
3,160件の閲覧回数
JohnKlug
Senior Contributor I

The manual:

i.MX Yocto Project User's Guide, Rev. L4.9.88_2.0.0-ga, 05/2018

Refers to a server that no longer exists for the build:

repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -m imx-4.9.88-2.0.0_ga.xml


Here is the manual:
i.MX Yocto Project User's Guide 

0 件の賞賛
返信
1 解決策
3,139件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

You can refer to the README file inside of Kirkstone's branch.

https://github.com/nxp-imx/imx-manifest/tree/imx-linux-kirkstone

To download the 5.15.71-2.2.0 release

$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.71-2.2.0.xml

To download the 5.15.52-2.1.0 release

$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.52-2.1.0.xml

To download the 5.15.32-2.0.0 release

$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.32-2.0.0.xml

Setup the build folder for a BSP release:

Note: The remaining instructions are for setting up a BSP release only. For setting up a demo, please see imx-manifest/README-<demo> for further instructions.

$: [MACHINE=<machine>] [DISTRO=fsl-imx-<backend>] source ./imx-setup-release.sh -b bld-<backend>

<machine>   defaults to `imx6qsabresd`
<backend>   Graphics backend type
    xwayland    Wayland with X11 support - default distro
    wayland     Wayland
    fb          Framebuffer (not supported for mx8)

Note if the poky community distro is used then build breaks will happen with some components using our meta-imx layer.

Examples:

  • Setup for XWayland.
$: MACHINE=imx8mnevk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland

Build an image:

$: bitbake <image recipe>

Some image recipes:

Image Name Description
imx-image-core core image with basic graphics and no multimedia
imx-image-multimedia image with multimedia and graphics
imx-image-full image with multimedia and machine learning and Qt

元の投稿で解決策を見る

3 返答(返信)
3,153件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello!

Now NXP did a migration to github from codeaurora. You can find the correct repo:

https://github.com/nxp-imx/imx-manifest/tree/imx-linux-rocko

It is possible that some branches does not work yet, but we are working solve the issues.

 

Best regards!

0 件の賞賛
返信
3,142件の閲覧回数
JohnKlug
Senior Contributor I
Rocko is EOL as is the 4.9 kernel.

The documentation says to use the following XML file with the repo command:
imx-4.9.88-2.0.0_ga.xml

However, if I choose imx-linux-kirkstone there is nothing ending in ga.

Which XML file for kirkstone would be appropriate for the MCIM6ULL-EVK to build an SD card image?

0 件の賞賛
返信
3,140件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

You can refer to the README file inside of Kirkstone's branch.

https://github.com/nxp-imx/imx-manifest/tree/imx-linux-kirkstone

To download the 5.15.71-2.2.0 release

$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.71-2.2.0.xml

To download the 5.15.52-2.1.0 release

$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.52-2.1.0.xml

To download the 5.15.32-2.0.0 release

$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.32-2.0.0.xml

Setup the build folder for a BSP release:

Note: The remaining instructions are for setting up a BSP release only. For setting up a demo, please see imx-manifest/README-<demo> for further instructions.

$: [MACHINE=<machine>] [DISTRO=fsl-imx-<backend>] source ./imx-setup-release.sh -b bld-<backend>

<machine>   defaults to `imx6qsabresd`
<backend>   Graphics backend type
    xwayland    Wayland with X11 support - default distro
    wayland     Wayland
    fb          Framebuffer (not supported for mx8)

Note if the poky community distro is used then build breaks will happen with some components using our meta-imx layer.

Examples:

  • Setup for XWayland.
$: MACHINE=imx8mnevk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland

Build an image:

$: bitbake <image recipe>

Some image recipes:

Image Name Description
imx-image-core core image with basic graphics and no multimedia
imx-image-multimedia image with multimedia and graphics
imx-image-full image with multimedia and machine learning and Qt