The manual:
i.MX Yocto Project User's Guide, Rev. L4.9.88_2.0.0-ga, 05/2018
Refers to a server that no longer exists for the build:
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-rocko -m imx-4.9.88-2.0.0_ga.xml
Here is the manual:
i.MX Yocto Project User's Guide
解決済! 解決策の投稿を見る。
You can refer to the README file inside of Kirkstone's branch.
https://github.com/nxp-imx/imx-manifest/tree/imx-linux-kirkstone
To download the 5.15.71-2.2.0 release
$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.71-2.2.0.xml
To download the 5.15.52-2.1.0 release
$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.52-2.1.0.xml
To download the 5.15.32-2.0.0 release
$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.32-2.0.0.xml
Note: The remaining instructions are for setting up a BSP release only. For setting up a demo, please see imx-manifest/README-<demo>
for further instructions.
$: [MACHINE=<machine>] [DISTRO=fsl-imx-<backend>] source ./imx-setup-release.sh -b bld-<backend>
<machine> defaults to `imx6qsabresd`
<backend> Graphics backend type
xwayland Wayland with X11 support - default distro
wayland Wayland
fb Framebuffer (not supported for mx8)
Note if the poky community distro is used then build breaks will happen with some components using our meta-imx
layer.
Examples:
$: MACHINE=imx8mnevk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland
$: bitbake <image recipe>
Some image recipes:
Image Name | Description |
---|---|
imx-image-core | core image with basic graphics and no multimedia |
imx-image-multimedia | image with multimedia and graphics |
imx-image-full | image with multimedia and machine learning and Qt |
Hello!
Now NXP did a migration to github from codeaurora. You can find the correct repo:
https://github.com/nxp-imx/imx-manifest/tree/imx-linux-rocko
It is possible that some branches does not work yet, but we are working solve the issues.
Best regards!
You can refer to the README file inside of Kirkstone's branch.
https://github.com/nxp-imx/imx-manifest/tree/imx-linux-kirkstone
To download the 5.15.71-2.2.0 release
$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.71-2.2.0.xml
To download the 5.15.52-2.1.0 release
$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.52-2.1.0.xml
To download the 5.15.32-2.0.0 release
$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.32-2.0.0.xml
Note: The remaining instructions are for setting up a BSP release only. For setting up a demo, please see imx-manifest/README-<demo>
for further instructions.
$: [MACHINE=<machine>] [DISTRO=fsl-imx-<backend>] source ./imx-setup-release.sh -b bld-<backend>
<machine> defaults to `imx6qsabresd`
<backend> Graphics backend type
xwayland Wayland with X11 support - default distro
wayland Wayland
fb Framebuffer (not supported for mx8)
Note if the poky community distro is used then build breaks will happen with some components using our meta-imx
layer.
Examples:
$: MACHINE=imx8mnevk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland
$: bitbake <image recipe>
Some image recipes:
Image Name | Description |
---|---|
imx-image-core | core image with basic graphics and no multimedia |
imx-image-multimedia | image with multimedia and graphics |
imx-image-full | image with multimedia and machine learning and Qt |