How did i write and read IPU2's regs in uboot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How did i write and read IPU2's regs in uboot?

跳至解决方案
1,035 次查看
wyb0116
Contributor II

I have a problem when debug imx6dq chips, when i use uboot command "mw" writing 0x02a0_0000 Configuration Register (IPU2_CONF) the uboot program will die. it means IPU2's reg can not write or read any time in uboot? or may be has another way to write and read IPU2's regs?

please help me.

标签 (3)
0 项奖励
回复
1 解答
927 次查看
igorpadykov
NXP Employee
NXP Employee

Hi wang

please check that ipu2 clocks are  enabled in CCM Clock Gating Registers 

(CCM_CCGR3).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
928 次查看
igorpadykov
NXP Employee
NXP Employee

Hi wang

please check that ipu2 clocks are  enabled in CCM Clock Gating Registers 

(CCM_CCGR3).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------