How did i write and read IPU2's regs in uboot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How did i write and read IPU2's regs in uboot?

ソリューションへジャンプ
1,167件の閲覧回数
wyb0116
Contributor II

I have a problem when debug imx6dq chips, when i use uboot command "mw" writing 0x02a0_0000 Configuration Register (IPU2_CONF) the uboot program will die. it means IPU2's reg can not write or read any time in uboot? or may be has another way to write and read IPU2's regs?

please help me.

ラベル(3)
0 件の賞賛
返信
1 解決策
1,059件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wang

please check that ipu2 clocks are  enabled in CCM Clock Gating Registers 

(CCM_CCGR3).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,060件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wang

please check that ipu2 clocks are  enabled in CCM Clock Gating Registers 

(CCM_CCGR3).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------