How change the PLL2_PFD0 frequency under Linux OS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How change the PLL2_PFD0 frequency under Linux OS

3,631件の閲覧回数
mzl
Contributor I

On my PCBA design based on i.MX6ULL. the base system is Linux OS.

Now we measured the DDR frequency with Oscilloscope and confirmed it's 307MHz. Then we read the register's value of CBCDR, CBCMR and CCM_ANALOG_PFD_528n and got the following value:

Value at address 0x20C4014 (0x76fc6014): 0x98D00

Value at address 0x20C4018 (0x76f80018): 0x24429324

Value at address 0x20C8100 (0x76fed100): 0xD018D05F

Value at address 0x20C8104 (0x76f9c104): 0xD0D8D05F

Value at address 0x20C8108 (0x76fc9108): 0xD098D05F

Value at address 0x20C810C (0x76f0c10c): 0xD098D05F

From the above registers' values, the DDR clock derived from PLL2_PFD0, and the PLL2_PFD0 frequency is 307MHz, which means that the DDR clock frequency is also configured to be 307MHz, the measured frequency from Oscilloscope matches the register configuration.

Now we want to improve the PLL2_PFD0 to be 396MHz so that the DDR clock frequency can be raised to 396MHz, in Linux system, how can we change the PLL2_PFD0 frequency? Thanks.

0 件の賞賛
返信
5 返答(返信)

3,499件の閲覧回数
mzl
Contributor I

Hello, Anybody can give a help on the above new findings? Thanks a lot for the support.

0 件の賞賛
返信

3,599件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

in linux kernel, the pll is defined in the clock driver

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/clk/imx/clk-imx6ul.c

hws[IMX6UL_CLK_PLL2_PFD0] = imx_clk_hw_pfd("pll2_pfd0_352m", "pll2_bus", base + 0x100, 0);
hws[IMX6UL_CLK_PLL2_PFD1] = imx_clk_hw_pfd("pll2_pfd1_594m", "pll2_bus", base + 0x100, 1);
hws[IMX6UL_CLK_PLL2_PFD2] = imx_clk_hw_pfd("pll2_pfd2_396m", "pll2_bus", base + 0x100, 2);
hws[IMX6UL_CLK_PLL2_PFD3] = imx_clk_hw_pfd("pll2_pfd3_594m", "pll2_bus", base + 0x100, 3);

 

0 件の賞賛
返信

3,524件の閲覧回数
mzl
Contributor I

Hello, from the clock tree read from our PCBA. Now we got the following values:

clock tree read.PNG

The value 306580645 actually matches with the DDR frequency measured on our PCBA (about 307MHz).

So my question is: where could I change this value? Thanks a lot.

0 件の賞賛
返信

3,493件の閲覧回数
mzl
Contributor I

Could anybody give some help on the new findings? Thanks a lot for the support.

0 件の賞賛
返信

3,383件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信