How can we interface a Smart Card with iMX6 DualLite processor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can we interface a Smart Card with iMX6 DualLite processor?

1,331 Views
admin
Specialist II

My Smart  Card on one side interfaces the card and on the other side it interfaces the processor. Clock, I/O and reset signal are supposed to come from the processor. Now to which exact pin it has to be connected with processor?

Labels (6)
Tags (2)
0 Kudos
Reply
1 Reply

1,114 Views
MehmetAliIpin
Contributor V

Dear Vinit,

It depends which smart card phy chip you are using, but at least to select the operaing voltage of 1.8,3.3, or 5 Volts, you need to add two more IO pins. If you write your phy chip, I will try to help you.

Mehmet Ali Ipin

0 Kudos
Reply