How can we interface a Smart Card with iMX6 DualLite processor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can we interface a Smart Card with iMX6 DualLite processor?

1,743件の閲覧回数
admin
Specialist II

My Smart  Card on one side interfaces the card and on the other side it interfaces the processor. Clock, I/O and reset signal are supposed to come from the processor. Now to which exact pin it has to be connected with processor?

ラベル(6)
タグ(2)
0 件の賞賛
返信
1 返信

1,526件の閲覧回数
MehmetAliIpin
Contributor V

Dear Vinit,

It depends which smart card phy chip you are using, but at least to select the operaing voltage of 1.8,3.3, or 5 Volts, you need to add two more IO pins. If you write your phy chip, I will try to help you.

Mehmet Ali Ipin

0 件の賞賛
返信