How can our device(IMX6DL) support iBeacon feature?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can our device(IMX6DL) support iBeacon feature?

Jump to solution
1,178 Views
jeyzhou
Contributor I

Hi,

  We use IMX6DL + Android 4.4, and we want to support the feature iBeacon to broadcast advertisement.

  How much effort for the iBeacon feature?

  If we upgrade the codebase to Android5.0, shall we pay any more effort for this feature like modifying Bluetooth stack or Bluetooth controller firmware?

  Thank you.

Best Regards,

Jey

Labels (2)
0 Kudos
Reply
1 Solution
1,078 Views
art
NXP Employee
NXP Employee

Freescale does not provide any special support for iBeacon feature. You may wait for official Android 5.0 BSP release from Freescale (end of Q2 2015) and then evaluate the feature with any Bluetooth LE compatible transceiver.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,079 Views
art
NXP Employee
NXP Employee

Freescale does not provide any special support for iBeacon feature. You may wait for official Android 5.0 BSP release from Freescale (end of Q2 2015) and then evaluate the feature with any Bluetooth LE compatible transceiver.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply