I am trying to take a screenshot using the "PrtScn" button on my keyboard with the Freescale SABRE i.MX6 Software development board that was programmed with the following image:
fsl-L3.14.28_1.0.0_iMX6qdls_Bundle/L3.14.28_1.0.0_ga_images_MX6/fsl-image-qt5-x11-imx6qdlsolo.sdcard
This gives me the following version of Linux:
sh-4.3# cat /proc/version
Linux version 3.14.28-1.0.0_ga+g91cf351 (jenkins@scmbl1) (gcc version 4.9.1 (GCC) ) #1 SMP PREEMPT Fri Mar 20 21:49:03 CST 2015
sh-4.3# cat /etc/issue
Poky (Yocto Project Reference Distro) 1.7 \n \l
Why does the screen shot functionality not work? Is there a way to take a screen shot by calling a command in the terminal?
解決済! 解決策の投稿を見る。
In the console type
export DISPLAY=:0
screenshot abc.png
Thank you, this works really great.
It works from the device as well as the USB-to-UART debug terminal connection. It is very helpful.
I've got a USB keyboard connected to the USB OTG port on the board. The USB keyboard has a USB hub on it where I have connected the mouse which works great. I've also tried connecting a USB flash drive to the keyboard, but I don't see Poky mounting this USB drive under /media or /mnt directory. Do you know how to manually figure out if Freescale SABRE i.MX 6 can see this device?
I'm trying to transfer the screenshot to a USB drive.
actually, when you plugin a device it will print out, even it is connected through a hub.
oot@imx6qsabresd:/unit_tests# usb 2-1.4: new high-speed USB device number 5 using ci_hdrc
usb-storage 2-1.4:1.0: USB Mass Storage device detected
scsi3 : usb-storage 2-1.4:1.0
scsi 3:0:0:0: Direct-Access Generic Flash Disk 8.07 PQ: 0 ANSI: 4
sd 3:0:0:0: [sda] 31457280 512-byte logical blocks: (16.1 GB/15.0 GiB)
sd 3:0:0:0: [sda] Write Protect is off
sd 3:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA
sda:
sd 3:0:0:0: [sda] Attached SCSI removable disk
Maybe you have some changes in the kernel make it slient.
you can type echo 8 > /proc/sys/kernel/printk to get the printk to print out more information. please make sure you haven't disabled the printk in kernel. By default, it is enabled.
to check if the i.MX6 see the device.
you also can type dmesg.
for hotplug you need to configure the udev configuration file
/etc/udev/udev.conf
Hello Kris Zawada,
The print screen button is not supported on the available images. You would need to add the support for this feature.
I would recommend looking for available applications that can be added to your Linux distribution. For example, as part of the FSL Release BSP you may find the sato-screenshot package that can be added although I haven’t tested it.
You may find more information on this specific package on the link below. You would need a simple capture utility similar to this one.