How can imx6 u-boot (u-boot 2014) support boot raw kernel image?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can imx6 u-boot (u-boot 2014) support boot raw kernel image?

Jump to solution
2,304 Views
zhanxiaozhang
Contributor III

Hi,I now optimize the imx6 boot time (yocto  ),with the fb backend ,the vivi_launcher can show image about 3s ,but I found the "starting kernel " stuck for 1s,can I use raw kernel image and reduce the boot time? So ,with this u-boot ,how can I boot the raw kernel image(kernel 3.10.53)?

Labels (4)
0 Kudos
Reply
1 Solution
2,084 Views
zhanxiaozhang
Contributor III

1: cannce bootz ( let uboot recognize Image as uImage)

mkimage -A arm -O linux -T kernel -C none -a 0x10008000 -e 0x10008000 -n 'TestImage' -d arch/arm/boot/Image arch/arm/boot/uImage

2: bootm 12000000 - 12c00000

It seems there no obviously boot time reducing between using zImage & Image

View solution in original post

0 Kudos
Reply
1 Reply
2,085 Views
zhanxiaozhang
Contributor III

1: cannce bootz ( let uboot recognize Image as uImage)

mkimage -A arm -O linux -T kernel -C none -a 0x10008000 -e 0x10008000 -n 'TestImage' -d arch/arm/boot/Image arch/arm/boot/uImage

2: bootm 12000000 - 12c00000

It seems there no obviously boot time reducing between using zImage & Image

0 Kudos
Reply