How can i get video from VCAM-AR1335B by using GStreamer in owr Yocto distro in DART-MX8M-PLUS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can i get video from VCAM-AR1335B by using GStreamer in owr Yocto distro in DART-MX8M-PLUS

961 Views
Zenik
Contributor I

I must to get video from VCAM-AR1335B (daA4200-30mci) by using GStreamer in owr Yocto distro, but when i try to execute follow command "gst-launch-1.0 v4l2src device=/dev/video1 ! videoconvert ! autovideosink" i see in console:

"

Setting pipeline to PAUSED ...

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

"

but after that nothing will be happend, but the same command works with VCAM-AR0821B.

Also both cameras work with Pylon app from Basler. I've built a Yocto distro via this manuals: 
"https://variwiki.com/index.php?title=MX8_Basler_Camera&release=mx8mp-yocto-hardknott-5.10.72_2.2.1-v... https://variwiki.com/index.php?title=MX8_Basler_Camera&release=RELEASE_ZEUS_V3.1_DART-MX8M-PLUS"

Can you help me with correct GStreamer command for getting realtime video from VCAM-AR1335B ?

0 Kudos
Reply
2 Replies

944 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If any pipeline works you can to build the driver for it:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/GStreamer-i-MX6-Pipelines/ta-p/1118160

 

Regards

0 Kudos
Reply

933 Views
Zenik
Contributor I

Hello,

It doesn't work correctly and i want to output video from VCAM-AR1335B to my display in real live. Can you share any resourses where i can read about it or find correct command? i have Yocto distro and i.mx8 processor on DART-MX8M-PLUS

About your previous manual....there are no some modules to execute it

Regards

0 Kudos
Reply