How can I rotate Wayland weston?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I rotate Wayland weston?

23,125 次查看
hyobokahn
Contributor II

Hello.

My project need to rotate screen.

I use Yocto git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga release version with Wayland backend and Qt5.

What is best way to rotate 90 degree clock-wise ?

I try to use weston.init (I add my self) with my display is LVDS 1024x768.

    [output]

   name=LVDS1

   mode=1024x768

   tansform=90

but, that is not work. in this reason

I try name=WL1, but it was not work too.

I see manual, if I use name=LVDS1, I must use drm or x11 backend.

So, I add [core] section with backend option like as

   [core]

   backend=drm-backend.so.

but, If I use this option, I fail to loading dri/swrast_dri.so,  dri/vivante_dri.so.

how can I install this library with Waland backend Yocto build system?

or, is there any better way to rotate screen without this way?

Thanks.

标签 (2)
标记 (1)
8 回复数

20,179 次查看
grigoritimonen
Contributor II

Finally I got it working.

The problem was in wrong connector name in the weston.ini.

root@imx8mmevk:~# ls /sys/class/drm/
card0  card0-DSI-1  version

I was trying to use card0 and card0-DSI-1 as a KMS connector names in the weston.ini. Then I took a look at /var/log/weston.log and found that proper name is DSI-1.

[05:55:41.223] DRM: head 'DSI-1' found, connector 33 is connected, EDID make 'unknown', model 'unknown', serial 'unknown'
[05:55:41.223] Registered plugin API 'weston_drm_output_api_v1' of size 24
[05:55:41.224] Chosen EGL config details:
               RGBA bits: 8 8 8 0
               swap interval range: 1 - 60
[05:55:41.224] No backlight control for output 'DSI-1'
[05:55:41.224] Output DSI-1 (crtc 31) video modes:
               720x1280@58.1, preferred, current, 67.3 MHz
[05:55:41.224] associating input device event0 with output DSI-1 (none by udev)
[05:55:41.224] associating input device event1 with output DSI-1 (none by udev)
[05:55:41.224] associating input device event2 with output DSI-1 (none by udev)
[05:55:41.224] Output 'DSI-1' enabled with head(s) DSI-1

So 'card0' part of name should be omitted.

Rotation works properly for me with following weston.ini:

root@imx8mmevk:~# cat /etc/xdg/weston/weston.ini
[core]
# i.MX: Disable idle timeout
idle-time=0
backend=drm-backend.so

[libinput]
touchscreen_calibrator=true

[output]
name=DSI-1
mode=720x1280@60
transform=270

[screen-share]
command=/usr/bin/weston --backend=rdp-backend.so --shell=fullscreen-shell.so --no-clients-resize

20,179 次查看
furkancanby
Contributor I


fbdev.jpg
I found the device name at "/var/log/weston.log". 
And I add these lines to  "/etc/xdg/weston/weston.ini" : 

(My default screen size :1024x768 and 60Hz)

[output]
name=fbdev
mode=768x1024@60
transform=270

You can set "transform" 90 or 270 to use your display vertical. 

Thank you.

0 项奖励
回复

20,164 次查看
joanxie
NXP TechSupport
NXP TechSupport

one can use xrandr to rotate the display, for more detailed information, pls refer to the chapter 5.2 XRandR of enclosed file.

0 项奖励
回复

20,163 次查看
hyobokahn
Contributor II

Hello Joan.

Thanks for your reply.

Frankly speaking, I know the way to use XRandR, but when I use x11 backend, the Qt application have window border on the top.

But, I do not want border. I want full screen with my own Qt application without any X11 window border.

may I know I can I remove it?

0 项奖励
回复

20,163 次查看
grigoritimonen
Contributor II

I have this problem too. Transform option doesn't seem to work on IMX8M Mini.

0 项奖励
回复

20,164 次查看
joanxie
NXP TechSupport
NXP TechSupport

for rotation, one also can use IPU, I send the sample code to you for reference

GitHub - jerome-pouiller/mxc-video-rotate 

0 项奖励
回复

20,165 次查看
erhany
Contributor II

Can you able to solve the issue? I am using imx6ul and have the same issue. transform parameter is not working with the default bsp. 

0 项奖励
回复

16,388 次查看
darsh_dev
Contributor V

Its worked, With below changes /etc/xdg/weston/weston.ini

[output]
name=DSI-1
mode=720x1280@60
transform=rotate-180

0 项奖励
回复