How can I output sound simultaneously to the hdmi sound and the internal sound of Imx6q?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How can I output sound simultaneously to the hdmi sound and the internal sound of Imx6q?

跳至解决方案
2,008 次查看
jongjupark
Contributor I

Dear community,

How can I output sound simultaneously to the hdmi sound and the internal sound of Imx6q?

Is there a hdmi sound source to write i2s?

please answer about my question.

 

**description**

Kernel Version : L3.14.28

Application : QT

标签 (1)
0 项奖励
回复
1 解答
1,923 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jongju

seems custom driver should be designed for such use case, please use

description of hdmi audio driver in sect.16.2.5 Audio attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,924 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jongju

seems custom driver should be designed for such use case, please use

description of hdmi audio driver in sect.16.2.5 Audio attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,923 次查看
jongjupark
Contributor I

Thank you. Your answer ^^

I need to create the necessary driver.

0 项奖励
回复