How can I output sound simultaneously to the hdmi sound and the internal sound of Imx6q?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I output sound simultaneously to the hdmi sound and the internal sound of Imx6q?

ソリューションへジャンプ
1,832件の閲覧回数
jongjupark
Contributor I

Dear community,

How can I output sound simultaneously to the hdmi sound and the internal sound of Imx6q?

Is there a hdmi sound source to write i2s?

please answer about my question.

 

**description**

Kernel Version : L3.14.28

Application : QT

ラベル(1)
0 件の賞賛
返信
1 解決策
1,747件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jongju

seems custom driver should be designed for such use case, please use

description of hdmi audio driver in sect.16.2.5 Audio attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,748件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jongju

seems custom driver should be designed for such use case, please use

description of hdmi audio driver in sect.16.2.5 Audio attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,747件の閲覧回数
jongjupark
Contributor I

Thank you. Your answer ^^

I need to create the necessary driver.

0 件の賞賛
返信