How can I create a patch for .config in my custom layer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I create a patch for .config in my custom layer

ソリューションへジャンプ
1,088件の閲覧回数
Derek0902
Contributor II

Hi,

 

After I modified kernel config use this command below, there is a .config in <build_dir>/tmp/work/imx8mqevk-poky-linux/linux-imx/6.1.36+gitAUTOINC+04b05c5527-r0/build

 

$ bitbake linux-imx -c menuconfig 

 

Then I override defconfig with .config and create a patch in my custom layer. But it didn't take effect in my board.

 

$ cp .config <build_dir>/tmp/work/imx8mqevk-poky-linux/linux-imx/6.1.36+gitAUTOINC+04b05c5527-r0/git/arch/arm64/configs/defconfig

 

 

I want to create a patch for this config in my custom layer. How can I do that?

 

Thanks & Regards,

Derek Lin

ラベル(1)
0 件の賞賛
返信
1 解決策
1,045件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

HI, @Derek0902 

Sorry to reply late

1. Make sure you have added the configuration changes in your customization layer. This is usually done by adding a conf/layer.conf file, which is read during the build process.

2. In the top-level directory of your customization layer, run the following command to create the patch file:
bitbake-diff . > custom-layer-config-patch
3. This command compares the current.config file in your build directory with the prebuild pristine.config file and generates a patch file custom-layer-config-patch.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,046件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

HI, @Derek0902 

Sorry to reply late

1. Make sure you have added the configuration changes in your customization layer. This is usually done by adding a conf/layer.conf file, which is read during the build process.

2. In the top-level directory of your customization layer, run the following command to create the patch file:
bitbake-diff . > custom-layer-config-patch
3. This command compares the current.config file in your build directory with the prebuild pristine.config file and generates a patch file custom-layer-config-patch.

0 件の賞賛
返信
1,044件の閲覧回数
Derek0902
Contributor II

Hi @pengyong_zhang ,

 

Thanks for your help. I have found that is in ../source/meta-freescale/recipes-kernel/linux-imx_6.1.bb. 

KBUILD_DEFCONFIG:mx6-generic-bsp = "imx_v7_defconfig"
KBUILD_DEFCONFIG:mx7-generic-bsp = "imx_v7_defconfig"
KBUILD_DEFCONFIG:mx8-generic-bsp = "imx_v8_defconfig"
KBUILD_DEFCONFIG:mx9-generic-bsp = "imx_v8_defconfig"

I modified the kernel config successfully.

 

Thanks & Regards,

 

Derek Lin

 

 

 

 

0 件の賞賛
返信