How about Windows Embedded Standard 7?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How about Windows Embedded Standard 7?

ソリューションへジャンプ
1,840件の閲覧回数
JHY
Contributor IV

Hello, i.MX6 has BSP for linux, android, windows embedded compact and RTOS, I know.

But I find some interesting product in the web.
(below link)

They say it is possible to use Windows XP or WES7 in i,MX6.

So my question is this, are there third partys woking with WES7?



 

http://www.diamondsystems.com/files/binaries/QuantumiMX6datasheet.pdf



ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,735件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello JHY,

I'm not sure if that PDF refers to the i.MX6 when it says "quantum sbcs", i think it talks in general. I haven't seen yet windows xp or 7 for an i.MX6 product since those products are made for a different architecture (ARM vs x86)


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,736件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello JHY,

I'm not sure if that PDF refers to the i.MX6 when it says "quantum sbcs", i think it talks in general. I haven't seen yet windows xp or 7 for an i.MX6 product since those products are made for a different architecture (ARM vs x86)


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信