How about Windows Embedded Standard 7?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How about Windows Embedded Standard 7?

Jump to solution
1,832 Views
JHY
Contributor IV

Hello, i.MX6 has BSP for linux, android, windows embedded compact and RTOS, I know.

But I find some interesting product in the web.
(below link)

They say it is possible to use Windows XP or WES7 in i,MX6.

So my question is this, are there third partys woking with WES7?



 

http://www.diamondsystems.com/files/binaries/QuantumiMX6datasheet.pdf



Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,727 Views
SergioSolis
NXP Employee
NXP Employee

Hello JHY,

I'm not sure if that PDF refers to the i.MX6 when it says "quantum sbcs", i think it talks in general. I haven't seen yet windows xp or 7 for an i.MX6 product since those products are made for a different architecture (ARM vs x86)


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,728 Views
SergioSolis
NXP Employee
NXP Employee

Hello JHY,

I'm not sure if that PDF refers to the i.MX6 when it says "quantum sbcs", i think it talks in general. I haven't seen yet windows xp or 7 for an i.MX6 product since those products are made for a different architecture (ARM vs x86)


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply