So, I managed to get this working. The container format is a 0x20 byte header with the following fields.
========= UNSIGNED WORKING DDR4 HEADER (OR) IVT =========
header.tag: 0xd1
header.length: 0x2000
header.version: 0x41
entry: 0x912000
reserved1: 0x00
dcd_ptr: 0x00
boot_data_ptr: 0x911fe0
self: 0x911fc0
csf: 0x93d9c0
reserved2: 0x0
boot_data.start: 0x911fc0
boot_data.size: 0x2da00
boot_data.plugin: 0x0
Btw, I found the information I was looking for in the i.MX8M mini's reference manual - section 6.1.6 Program image (rather than the nano's).
PS: I put together a Rust implementation for the nano along with a working uart console. You can find the code here
Welcome to minicom 2.8
OPTIONS:
Compiled on Oct 25 2021, 04:59:49.
Port /dev/tty.usbserial-1101, 11:47:54
Press Meta-Z for help on special keys
[ 0.000002] imx8mn-rs version 0.1.0
[ 0.003485] Booting on: i.MX 8M Nano EVK
[ 0.007385] Current privilege level: EL3
[ 0.011295] Exception handling state:
[ 0.014934] Debug: Masked
[ 0.018143] SError: Unmasked
[ 0.021431] IRQ: Masked
[ 0.024728] FIQ: Masked
[ 0.027919] Drivers loaded:
[ 0.030685] 1. i.MX 8M Nano Uart2
[ 0.034428] Chars written: 388
[ 0.037546] Counter Control Register: 259
[ 0.041462]
[ 0.042998] ... wait forever