Hello Victor,
Actually you haven't answered my questions:
"Does NXP recommend using a heat sink with the IMX8M? If yes, which type is recommended?"
The AN12118.pdf states that the IMX8M power consumption can be as high as 3.82W, so under 30 centigrade ambient, the IMX8M junction temperature can be calculated as 93.4 centigrade, which is almost equal to the maximum IMX8M allowable value (95 centigrade). But the NXP documentations don't provide any recommendation on cooling the IMX8M.
Which heat sink is preferable for using with the IMX8M?
Which heat sink is safe to use with the IMX8M bare die package?
Best regards,
Vadim Aleynikov