Does NXP recommend using a heat sink with the IMX8M? If yes, which type is recommended?
Best regards,
Vadim Aleynikov
You can refer to "i.MX 8M Quad Power Consumption Measurement" Application Note
https://www.nxp.com/docs/en/nxp/application-notes/AN12118.pdf
regarding to estimation of heat dissipation.
Also please refer to "i.MX 6 Series Thermal Management Guidelines" Application Note:
http://www.nxp.com/assets/documents/data/en/application-notes/AN4579.pdf
for thermal estimations implementation.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Victor,
Actually you haven't answered my questions:
"Does NXP recommend using a heat sink with the IMX8M? If yes, which type is recommended?"
The AN12118.pdf states that the IMX8M power consumption can be as high as 3.82W, so under 30 centigrade ambient, the IMX8M junction temperature can be calculated as 93.4 centigrade, which is almost equal to the maximum IMX8M allowable value (95 centigrade). But the NXP documentations don't provide any recommendation on cooling the IMX8M.
Which heat sink is preferable for using with the IMX8M?
Which heat sink is safe to use with the IMX8M bare die package?
Best regards,
Vadim Aleynikov
I am especially interested in the maximum force the heatsink can press onto the processor. Is there any documentation on that?
Also you can refer EVK board design that has a radiator:
https://www.nxp.com/docs/en/user-guide/IMX8MDQLQEVKHUG.pdf
Hello Victor,
This User Guide doesn't contain data on the heatsink. The only mention about heatsink is the following:
It is strongly recommended to install fans on the heatsink to avoid any potential damages to the PCBA. You can get fans from www.nxp.com/i.MX8M.
The aforementioned link points to the main i.MX8M page which doesn't contain data either on fan or heatsink.
Best regards,
Vadim
Hello,
on EVK boards with recent release chips, there is no fan anymore, only passive cooling.
This is why the fan requirement is considered as obsolete and that may be the reason why
you cannot find it on the web.
Regards,
Yuri.
Hello,
On the NXP EVK, which we have, the iMX8M in the "VO" package (with a metal lid) is assembled and a mysterious " MBF25004" heat sink is used. In the current iMX8M datasheets, the only "VA" bare die package is available.
If using a heatsink on the bare die package is safe? If yes, which heatsink can be safely used?
Best regards,
Vadim
Hello,
The design files contain BOM.
https://www.nxp.com/webapp/Download?colCode=MCIMX8M-EVK-DESIGNFILES&appType=license
Regards,
Yuri.
Hello Yuri,
This design is well known fo me but unfortunately its BOM doesn't contain usable data on the processor heatsink. The processor/heatsink BOM row is as follows:
750-77879 | U101 | MIMX8MQ6DVAJZAA + MBF25004-15W/2.0P+T725 A1 | SUBASSEMBLY, IC CPU QUAD CORTEX A53+M4 1.5GHZ BGA621 + HEAT SINK, PUSH PIN BLACK ALUMINUM 14MM | SUBASSEBLY | 330-77069,901-76977 | bga621_heatsink |
The number in the first cell (750-77879) is an internal NXP number.
Searching for either MBF25004 and 30-77069 and 901-76977 doesn't result in any heatsink.
Best regards,
Vadim