I am debugging the wm8962 audio chip on the i.mx 6ull, and now I don't know why there is no sound from either the headphones or the speaker. By observing the log, it seems that there is a problem with the configuration of sai2. However, I have connected these pins of sai2 to the wm8960 audio chip and confirmed that there is no problem. Now I need to check whether there is a problem with my device tree configuration or the hardware device?
And here is my imx-fire-sound-wm8962-overlay.dts
/*
* Copyright (C) 2019 - All Rights Reserved by
* filename : imx-fire-mpu6050-overlay.dts
* brief : Device Tree overlay for EBF6ull Pro mpu6050 device
* author : embedfire
* date : 2019-11-26
* version : A001
*/
#include "../imx6ul-pinfunc.h"
#include "../imx6ull-pinfunc.h"
#include "dt-bindings/clock/imx6ul-clock.h"
/dts-v1/;
/plugin/;
/ {
fragment@1 {
target = <&i2c1>;
__overlay__ {
clock_frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c1>;
status = "okay";
#address-cells = <1>;
#size-cells = <0>;
codec: wm8962@1a {
compatible = "wlf,wm8962";
reg = <0x1a>;
clocks = <&clks IMX6UL_CLK_SAI2>;
clock-names = "mclk";
wlf,shared-lrclk;
// wlf,dc-servo-disable;
DCVDD-supply = <&dcvdd_reg>;
DBVDD-supply = <&dbvdd_reg>;
AVDD-supply = <&avdd_reg>;
CPVDD-supply = <&cpvdd_reg>;
MICVDD-supply = <&micvdd_reg>;
PLLVDD-supply = <&pllvdd_reg>;
SPKVDD1-supply = <&spkvdd1_reg>;
SPKVDD2-supply = <&spkvdd2_reg>;
amic-mono;
};
};
};
fragment@2{
target-path="/";
__overlay__{
sound {
compatible = "fsl,imx6ul-evk-wm8962",
"fsl,imx-audio-wm8962";
model = "wm8962-audio";
cpu-dai = <&sai2>;
audio-codec = <&codec>;
asrc-controller = <&asrc>;
gpr = <&gpr 4 0x100000 0x100000>;
/*
* hp-det = <hp-det-pin hp-det-polarity>;
* hp-det-pin: JD1 JD2 or JD3
* hp-det-polarity = 0: hp detect high for headphone
* hp-det-polarity = 1: hp detect high for speaker
*/
// hp-det = 1>;
/*hp-det-gpios = <&gpio5 4 0>;
mic-det-gpios = <&gpio5 4 0>;*/
audio-routing =
"Headphone Jack", "HPOUTL",
"Headphone Jack", "HPOUTR",
"Ext Spk", "SPKOUTL",
"Ext Spk", "SPKOUTR",
"AMIC", "MICBIAS",
"DMIC", "MICBIAS",
"DMICDAT", "DMIC",
"Playback", "CPU-Playback",
"CPU-Capture", "Capture";
status = "okay";
};
};
};
fragment@3{
target=<&iomuxc>;
__overlay__ {
pinctrl_i2c1: i2c1grp {
fsl,pins = <
MX6UL_PAD_UART4_TX_DATA__I2C1_SCL 0x4001b8b0
MX6UL_PAD_UART4_RX_DATA__I2C1_SDA 0x4001b8b0
>;
};
pinctrl_sai2: sai2grp {
fsl,pins = <
MX6UL_PAD_JTAG_TDI__SAI2_TX_BCLK 0x17088
MX6UL_PAD_JTAG_TDO__SAI2_TX_SYNC 0x17088
MX6UL_PAD_JTAG_TRST_B__SAI2_TX_DATA 0x11088
MX6UL_PAD_JTAG_TCK__SAI2_RX_DATA 0x11088
MX6UL_PAD_JTAG_TMS__SAI2_MCLK 0x17088
>;
};
};
};
fragment@4 {
target=<&sai2>;
__overlay__{
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai2>;
/*&pinctrl_sai2_hp_det_b>;*/
assigned-clocks = <&clks IMX6UL_CLK_SAI2_SEL>,
<&clks IMX6UL_CLK_SAI2>;
assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <0>, <12288000>;
status = "okay";
};
};
};
The log:
log
The hardware connection:
hardware connection
If you need more details, please tell me that.
Thanks.
已解决! 转到解答。
Hello,
I suggest you use our device tree as reference:
I see that you are not using mclk property to use it as output in SAI2 node, please check if this helps with your design.
I do not see issues in hardware connections.
Best regards.
Hello,
I suggest you use our device tree as reference:
I see that you are not using mclk property to use it as output in SAI2 node, please check if this helps with your design.
I do not see issues in hardware connections.
Best regards.
Your suggestion played a substantial role in my registration failure error, and also reminded me of the alias problem. The above error no longer appears, but now there is a problem with playing music. I think it is probably a problem with my hardware. I will check the WM8962 module problem myself. Thank you for your help.
The following figure shows the changes I made to the main device tree and the device tree overlay. I hope it can be used as a reference when others encounter this problem in the future.main device tree
device tree overlay
play error