Hardware encoding and display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hardware encoding and display

1,537件の閲覧回数
fabricelouveau
Contributor I

Hi everyone,

I try to capture a video from a webcam and display it on the screen using a SabreLite (imx6Q).

My webcam allow two mode of capture YUYV and MJPEG. As I want to use a 720p at 30 fps, I can only use MJPEG. (Logitech C270).

I find how to capture video and display it on the screen without any transcoding:

gst-launch-1.0 v4l2src ! "image/jpeg,width=1280, height=720,framerate=30/1" ! queue ! jpegdec ! imxg2dvideosink

This works. I try to use imxvpudec without any chance. no error message but no video displayed.

I want to convert my MJPEG into h264 using imxvpuenc_h264 and display it on the screen but I can't find the correct command line.

Can you help me ?

Fabrice

ラベル(4)
0 件の賞賛
返信
1 返信

1,354件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

The following Issues decoding MJPEG with VPUdec

may clarify situation.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信