Hardware Trigger for Image Capture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hardware Trigger for Image Capture

2,123件の閲覧回数
rajabalaji
Contributor II

Hi All,

In the example codes provided for image capture from OV5640 using imx6, i always see that the image capture is using v4l2 either being read from a older buffer or started with a software trigger. Is it possible to start a image capture using external hardware trigger? is there any driver or v4l2 limitation? is there a feature in ov5640 that can be used to achieve this?

I want the frame at a particular instant where the hardware trigger is happening. So it is not possible to start a capture from software in my application.

Thanks in advance!!

ラベル(2)
0 件の賞賛
返信
1 返信

1,769件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raja

one can try to use for such purpose CSIx_DATA_EN.

Also as sensor is master for synchronization signals, it can

provide ability for external sync. One can consult with sensor datasheet

for availability of such feature.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信