Hardware ECC Accelerator Layout Select Register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hardware ECC Accelerator Layout Select Register

ソリューションへジャンプ
1,590件の閲覧回数
takashitakahash
Contributor III

Hi community.

IMX6DQ RM of sect 17.6.7 Hardware ECC Accelerator Layout Select Register

of  (BCH_LAYOUTSELECT),

Desclibed in Chip Select of CS15 ~ CS0 , as the ball function of iMX6, it is only NAND_CE3 ~ CE0.

What is  CS15 ~ 0 ?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,453件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Only CS0-CS3 bit fields of  BCH_LAYOUTSELECT should be used for i.MX6
 
Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,454件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Only CS0-CS3 bit fields of  BCH_LAYOUTSELECT should be used for i.MX6
 
Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信