Hardware ECC Accelerator Layout Select Register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardware ECC Accelerator Layout Select Register

Jump to solution
1,219 Views
takashitakahash
Contributor III

Hi community.

IMX6DQ RM of sect 17.6.7 Hardware ECC Accelerator Layout Select Register

of  (BCH_LAYOUTSELECT),

Desclibed in Chip Select of CS15 ~ CS0 , as the ball function of iMX6, it is only NAND_CE3 ~ CE0.

What is  CS15 ~ 0 ?

Labels (2)
0 Kudos
Reply
1 Solution
1,082 Views
Yuri
NXP Employee
NXP Employee

  Only CS0-CS3 bit fields of  BCH_LAYOUTSELECT should be used for i.MX6
 
Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,083 Views
Yuri
NXP Employee
NXP Employee

  Only CS0-CS3 bit fields of  BCH_LAYOUTSELECT should be used for i.MX6
 
Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply