Hard to get android source(Android/kernel/U-boot)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hard to get android source(Android/kernel/U-boot)

ソリューションへジャンプ
4,857件の閲覧回数
conteczxy
Contributor III

I want to download i.MX6q Android O release source code.


I had Android proprietary source code package imx-o8.0.0_1.0.0 under the ~/. directory, and follow the steps below.

$mkdir ~/bin
$curl https://storage.googleapis.com/git-repo-downloads/repo
$chmod a+x ~/bin/repo
$export PATH=${PATH}:~/bin

$ source ~/imx-o8.0.0_1.0.0_ga/imx_android_setup.sh

During this process, it always stop continuing when output following messages.

Fetching project platform/external/mdnsresponder
Fetching project platform/packages/apps/SpareParts 10.00 KiB/s   
Fetching project platform/packages/apps/ProtipsiB | 5.00 KiB/s   
Fetching project device/generic/x86
Fetching projects:  28% (168/597)
Fetching project platform/external/toybox
Fetching project platform/external/libedit47 MiB | 10.00 KiB/s   
Fetching project platform/external/trappy79 MiB | 11.00 KiB/s     
Fetching project platform/external/ipsec-toolsiB | 10.00 KiB/s   
Fetching project platform/external/eigen
Fetching project aosp/platform/system/extras MiB | 10.00 KiB/s   
remote: Counting objects: 29086, done.        B | 7.00 KiB/s     
remote: Compressing objects: 100% (695/695), done.        /s     
error: RPC failed; curl 56 GnuTLS recv error (-54): Error in the pull function.
fatal: The remote end hung up unexpectedly
fatal: early EOF
fatal: index-pack failed
remote: Counting objects: 2923145, done.        
remote: Compressing objects: 100% (11444/11444), done.        
error: RPC failed; curl 56 GnuTLS recv error (-54): Error in the pull function.
fatal: The remote end hung up unexpectedly
fatal: early EOF
fatal: index-pack failed
error: RPC failed; curl 56 GnuTLS recv error (-54): Error in the pull function.
fatal: The remote end hung up unexpectedly
fatal: early EOF
fatal: index-pack failed
error: RPC failed; curl 56 GnuTLS recv error (-54): Error in the pull function.
fatal: The remote end hung up unexpectedly
fatal: early EOF
fatal: index-pack failed
remote: Counting objects: 29086, done.         KiB | 8.00 KiB/s    
remote: Counting objects: 226078, done.        KiB | 8.00 KiB/s   
remote: Compressing objects: 100% (695/695), done.        KiB/s   
remote: Compressing objects: 100% (158/158), done.        
remote: Counting objects: 614728, done.        
remote: Compressing objects: 100% (662/662), done.        
error: RPC failed; curl 56 GnuTLS recv error (-54): Error in the pull function.
fatal: The remote end hung up unexpectedly
fatal: early EOF
fatal: index-pack failed
error: Cannot fetch uboot-imx from https://source.codeaurora.org/external/imx/uboot-imx
Fetching project platform/hardware/qcom/msm8996
Fetching projects:  29% (174/597)
error: RPC failed; curl 56 GnuTLS recv error (-54): Error in the pull function.
fatal: The remote end hung up unexpectedly
fatal: early EOF
fatal: index-pack failed
error: Cannot fetch aosp/platform/packages/inputmethods/LatinIME from https://source.codeaurora.org/external/imx/aosp/platform/packages/inputmethods/LatinIME
error: RPC failed; curl 56 GnuTLS recv error (-54): Error in the pull function.
fatal: The remote end hung up unexpectedly
fatal: early EOF
fatal: index-pack failed
error: Cannot fetch aosp/platform/frameworks/base from https://source.codeaurora.org/external/imx/aosp/platform/frameworks/base

I am not sure what to do, has anyone met the same problem?

Thanks,

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
4,492件の閲覧回数
conteczxy
Contributor III

I found an article https://community.nxp.com/docs/DOC-340804  , it seems very helpful, I am going to have a try.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,493件の閲覧回数
conteczxy
Contributor III

I found an article https://community.nxp.com/docs/DOC-340804  , it seems very helpful, I am going to have a try.

0 件の賞賛
返信
4,492件の閲覧回数
b36401
NXP Employee
NXP Employee

It seems there is some issue with gnutls library.
Please update openssl and gnutls packages.
Also please try to reinstall git.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信