Hang in kernel and reboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hang in kernel and reboot

Jump to solution
1,467 Views
vinothkumars
Senior Contributor IV

Hi All,

 

Board hang in kernel and reboot. please find the below log and provide your feedback.

 

[ 5.826828] ++++++++++++++++ mxc_gpio_probe +++++++++++++++++++++
[ 5.832778] ++++++++++++++++ mxc_gpio_probe 1 +++++++++++++++++++++
[ 5.839236] ++++++++++++++++ mxc_gpio_probe 2 port->irq: 0x46 +++++++++++++++++++++
[ 5.847016] ++++++++++++++++ mxc_gpio_probe 3 port->clk: 0x0 +++++++++++++++++++++
[ 5.854745] ++++++++++++++++ mxc_gpio_probe 4 +++++++++++++++++++++
[ 5.861167] ++++++++++++++++ mxc_gpio_probe 5 +++++++++++++++++++++
[ 5.867606] ++++++++++++++++ mxc_gpio_probe 6 +++++++++++++++++++++
[ 5.874024] ++++++++++++++++ mxc_gpio_probe 7 +++++++++++++++++++++
[ 5.881132] ++++++++++++++++ mxc_gpio_probe 8 +++++++++++++++++++++
[ 5.887777] ++++++++++++++++ mxc_gpio_probe +++++++++++++++++++++
[ 5.893752] ++++++++++++++++ mxc_gpio_probe 1 +++++++++++++++++++++
[ 5.900166] ++++++++++++++++ mxc_gpio_probe 2 port->irq: 0x47 +++++++++++++++++++++
[ 5.907971] ++++++++++++++++ mxc_gpio_probe 3 port->clk: 0x0 +++++++++++++++++++++
[ 5.915699] ++++++++++++++++ mxc_gpio_probe 4 +++++++++++++++++++++
[ 5.922124] ++++++++++++++++ mxc_gpio_probe 5 +++++++++++++++++++++
[ 5.928557] Bad mode in Error handler detected on CPU0, code 0xbf000002 -- SError
[ 5.936013] Internal error: Oops - bad mode: 0 [#1] PREEMPT SMP
[ 5.941921] Modules linked in:
[ 5.944961] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.14.98-00053-g767bb3e-dirty #8
[ 5.952774] Hardware name: Freescale i.MX8QM MEK (DT)
[ 5.957815] task: ffff8008f60b8000 task.stack: ffff000008048000
[ 5.963732] PC is at mxc_gpio_probe+0x3f8/0x6cc
[ 5.968241] LR is at mxc_gpio_probe+0x3d8/0x6cc
[ 5.972758] pc : [<ffff0000084454f0>] lr : [<ffff0000084454d0>] pstate: 60000045
[ 5.980139] sp : ffff00000804bb70
[ 5.983442] x29: ffff00000804bb80 x28: 0000000000000000
[ 5.988740] x27: ffff000008ace330 x26: 0000000000000001
[ 5.994040] x25: ffff8008f670ec18 x24: ffff8008fffd3168
[ 5.999339] x23: ffff000008ace000 x22: ffff0000090ba000
[ 6.004638] x21: ffff8008f6657410 x20: ffff000009239000
[ 6.009938] x19: ffff8008f6657400 x18: 000000000000000e
[ 6.015237] x17: 0000000000000001 x16: 0000000000000019
[ 6.020536] x15: 0000000000000033 x14: 0d202b2b2b2b2b2b
[ 6.025836] x13: 2b2b2b2b2b2b2b2b x12: 519a55eb4866f100
[ 6.031135] x11: ffff00000804b860 x10: 00000000000008c0
[ 6.036435] x9 : ffff00000804b8c0 x8 : ffff8008f60b8920
[ 6.041734] x7 : ffff000008528bfc x6 : 0000000000000001
[ 6.047033] x5 : 0000000000000400 x4 : 0000000000000000
[ 6.052333] x3 : 0000000000000002 x2 : ffff00000c290000
[ 6.057632] x1 : ffff000009239898 x0 : ffff00000c290014
[ 6.062939]
[ 6.062939] X8: 0xffff8008f60b88a0:
[ 6.067885] 88a0 00000000 00000000 f6098180 ffff8008 00000001 00000000 00000000 00000000
[ 6.076049] 88c0 f60bd780 ffff8008 f60b8000 ffff8008 f60b8000 ffff8008 08ed6000 ffff0000
[ 6.084215] 88e0 090f5c88 ffff0000 00000001 00000000 f60b85a8 ffff8008 090ba000 ffff0000
[ 6.092383] 8900 08a652bc ffff0000 08a89000 ffff0000 0804b8c0 ffff0000 0804b8c0 ffff0000
[ 6.100548] 8920 0808606c ffff0000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.108714] 8940 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.116880] 8960 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.125047] 8980 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.133217]
[ 6.133217] X19: 0xffff8008f6657380:
[ 6.138252] 7380 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.146418] 73a0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.154584] 73c0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.162750] 73e0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.170917] 7400 f6648b00 ffff8008 ffffffff 00000000 0912ea90 ffff0000 f664a100 ffff8008
[ 6.179083] 7420 f6648b00 ffff8008 f6657828 ffff8008 f6657028 ffff8008 0912eaa0 ffff0000
[ 6.187249] 7440 f624e300 ffff8008 0912e480 ffff0000 f664b770 ffff8008 00000003 00000007
[ 6.195415] 7460 00000000 00000000 00000000 00000000 f60b8000 ffff8008 00000000 00000000
[ 6.203583]
[ 6.203583] X21: 0xffff8008f6657390:
[ 6.208620] 7390 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.216787] 73b0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.224953] 73d0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.233119] 73f0 00000000 00000000 00000000 00000000 f6648b00 ffff8008 ffffffff 00000000
[ 6.241285] 7410 0912ea90 ffff0000 f664a100 ffff8008 f6648b00 ffff8008 f6657828 ffff8008
[ 6.249452] 7430 f6657028 ffff8008 0912eaa0 ffff0000 f624e300 ffff8008 0912e480 ffff0000
[ 6.257618] 7450 f664b770 ffff8008 00000003 00000007 00000000 00000000 00000000 00000000
[ 6.265784] 7470 f60b8000 ffff8008 00000000 00000000 f6657480 ffff8008 f6657480 ffff8008
[ 6.273954]
[ 6.273954] X24: 0xffff8008fffd30e8:
[ 6.278989] 30e8 00000000 00000000 00000000 00000000 08ce9600 ffff0000 00000005 00000000
[ 6.287155] 3108 fffd3160 ffff8008 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.295322] 3128 f63f0580 ffff8008 00000124 00000000 00000005 00000000 00000000 00000000
[ 6.303488] 3148 087cc640 ffff0000 00000000 00000000 00000000 00000000 6f697067 00000000
[ 6.311654] 3168 fffd3698 ffff8008 08d77b70 ffff0000 0000002e 00000000 fffd3210 ffff8008
[ 6.319820] 3188 00000000 00000000 08b32d38 ffff0000 fffd3220 ffff8008 00000000 00000000
[ 6.327987] 31a8 fff596f0 ffff8008 00000000 00000000 fffd36a0 ffff8008 f63f0700 ffff8008
[ 6.336153] 31c8 fffd3700 ffff8008 fffd2c90 ffff8008 fff59748 ffff8008 f624ee00 ffff8008
[ 6.344320]
[ 6.344320] X25: 0xffff8008f670eb98:
[ 6.349358] eb98 00000000 00000000 f670e400 ffff8008 00000000 00000000 00000000 00000000
[ 6.357524] ebb8 00000000 00000000 f670e400 ffff8008 00000000 00000000 00000000 00000000
[ 6.365690] ebd8 00000000 00000000 f670e400 ffff8008 00000000 00000000 00000000 00000000
[ 6.373857] ebf8 00000000 00000000 f6865880 ffff8008 f66576a0 ffff8008 0859dcb8 ffff0000
[ 6.382023] ec18 00000000 00000000 00000000 00000000 00000000 00000000 0c290000 ffff0000
[ 6.390189] ec38 00000047 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.398355] ec58 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.406522] ec78 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 6.414691]
[ 6.416168] Process swapper/0 (pid: 1, stack limit = 0xffff000008048000)
[ 6.422857] Call trace:
[ 6.425291] Exception stack(0xffff00000804ba30 to 0xffff00000804bb70)
[ 6.431720] ba20: ffff00000c290014 ffff000009239898
[ 6.439537] ba40: ffff00000c290000 0000000000000002 0000000000000000 0000000000000400
[ 6.447356] ba60: 0000000000000001 ffff000008528bfc ffff8008f60b8920 ffff00000804b8c0
[ 6.455175] ba80: 00000000000008c0 ffff00000804b860 519a55eb4866f100 2b2b2b2b2b2b2b2b
[ 6.462993] baa0: 0d202b2b2b2b2b2b 0000000000000033 0000000000000019 0000000000000001
[ 6.470812] bac0: 000000000000000e ffff8008f6657400 ffff000009239000 ffff8008f6657410
[ 6.478633] bae0: ffff0000090ba000 ffff000008ace000 ffff8008fffd3168 ffff8008f670ec18
[ 6.486449] bb00: 0000000000000001 ffff000008ace330 0000000000000000 ffff00000804bb80
[ 6.494268] bb20: ffff0000084454d0 ffff00000804bb70 ffff0000084454f0 0000000060000045
[ 6.502087] bb40: 0000000000000006 0000000000000040 ffffffffffffffff 656b61774809001e
[ 6.509905] bb60: ffff00000804bb80 ffff0000084454f0
[ 6.514774] [<ffff0000084454f0>] mxc_gpio_probe+0x3f8/0x6cc
[ 6.520338] [<ffff00000859c410>] platform_drv_probe+0x50/0xc8
[ 6.526067] [<ffff00000859a370>] driver_probe_device+0x258/0x30c
[ 6.532060] [<ffff00000859a4d0>] __driver_attach+0xac/0xb0
[ 6.537534] [<ffff000008598064>] bus_for_each_dev+0x64/0xb4
[ 6.543091] [<ffff000008599c24>] driver_attach+0x20/0x28
[ 6.548391] [<ffff000008599798>] bus_add_driver+0x1c4/0x228
[ 6.553953] [<ffff00000859b270>] driver_register+0x74/0x10c
[ 6.559511] [<ffff00000859c354>] __platform_driver_register+0x4c/0x54
[ 6.565947] [<ffff000008e55b68>] gpio_mxc_init+0x18/0x20
[ 6.571245] [<ffff000008083ca0>] do_one_initcall+0x48/0x14c
[ 6.576805] [<ffff000008e20df0>] kernel_init_freeable+0x13c/0x1d8
[ 6.582887] [<ffff000008a6159c>] kernel_init+0x10/0x13c
[ 6.588095] [<ffff000008084f14>] ret_from_fork+0x10/0x18
[ 6.593398] Code: b9401400 8b000040 b900001f d5033e9f (f9400420)
[ 6.599486] ---[ end trace d172ca0f1ca74470 ]---
[ 6.604100] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 6.604100]
[ 6.613204] Rebooting in 5 seconds..

 

 

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply
1 Solution
1,450 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

from "mxc_gpio_probe" log seems there is problem with gpio, one can check if

that gpio is owned by m4 partition, use flexcan example on link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Resource-...

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
1,451 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

from "mxc_gpio_probe" log seems there is problem with gpio, one can check if

that gpio is owned by m4 partition, use flexcan example on link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Resource-...

 

Best regards
igor

0 Kudos
Reply