HSIC imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HSIC imx6

3,743 次查看
cdav
Contributor I

Hi all, I have issue about HSIC link on H2. We follow the method described in https://community.freescale.com/servlet/JiveServlet/download/302256-251494/USB_HOST2_initial_setting... but nothing in ouput. Please, let me know what we have to set exactly to have this link running.Thanks in advance. Best regards

标签 (1)
0 项奖励
回复
2 回复数

2,688 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Claudette,

The file that you mention it was provided by the customer mention that it was not working, if you review the following thread,

Need proper initialization for USB Host2 (HSIC) in i.MX6x

You are going to find instructions to add the Host2 support using Linux. But the file it is for WINCE.

0 项奖励
回复

2,687 次查看
cdav
Contributor I

Hello,

Thank you for your reply.

We started from the mentioned file but we apply also the items from Junjie Liu answer.

Even if the file is for Wince, I guess the different steps of initialization for this interface are same even if the implementation differs.

Could you provide exactly what to do to implement the HSIC on H2 ? Have you a code example even if it is not under Linux ?

Best regards

De : jamesbone

Envoyé : mardi 2 décembre 2014 18:44

À : DAVID Claudette

Objet : Re: - HSIC imx6

<https://community.freescale.com/>

HSIC imx6

reply from jamesbone<https://community.freescale.com/people/jamesbone?et=watches.email.thread> in i.MX Community - View the full discussion<https://community.freescale.com/message/459158?et=watches.email.thread#459158>

0 项奖励
回复